Skip to main content
Associate II
October 28, 2024
Question

SPL support for STEVAL-ESC001V1 or X-NUCLEO-IHM08M1?

  • October 28, 2024
  • 0 replies
  • 585 views

Hello.

Is there an example F/W for STEVAL-ESC001V1 or X-NUCLEO-IHM08M1 that is SPL compatible?
I need to continue to use the Standard Peripheral Library (SPL) to utilize the existing code.
If there is a way to create or convert the project by X-CUBE-MCSDK to SPL compatible, that would be the best.

Thank you!

This topic has been closed for replies.