STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

nucleo-144stm32f429 usb otg fs

Posted on June 06, 2018 at 21:58Hello, I check stm32cube-fw-f4-v1.21 library for nucleo-144stm32f429zi, I can't find a sample for usb-otg-fs, does anybody be able to provide a sample?also when I try to configure nucleo-144stm32f429zi in stm32cube, I...

yang hong by Associate III
  • 609 Views
  • 1 replies
  • 0 kudos

uart/usart communication

Posted on June 06, 2018 at 22:01I am using nucleo-144stm32f429zi uart and usart. I want to create a rs485 serial communication. Can I connect FTDI USB-RS485-WE-1800-BT directly to nucleo-144 uart/usart port? FTDI CABLE IS 5VDC? nucleo-144stm32f429zi...

yang hong by Associate III
  • 528 Views
  • 1 replies
  • 0 kudos

Ethernet Layer 2 Broadcast

Posted on June 04, 2018 at 20:29Hello Everyone,I need help to send data packets on Ethernet but i want to broadcast it to all the other device on network. For now i want to send hardcoded data which later could be changed. In STMcubeMx i've checked ...

Resolved! STM32L4x6 GPIO PA3 Reset Value

Posted on June 01, 2018 at 15:36 Hi guys, I'm having some troubles understanding the behavior of the ST GPIO on start-up, specifically PA3 on STM32L496VE micro. Background: I'm trying to program/flash a SiLabs BT121 (Bluetooth module) chip an...

0690X0000060KwwQAE.png 0690X0000060L4VQAU.png 0690X0000060L4MQAU.png 0690X0000060KskQAE.png

How to manage SPI transmission using RTX

Posted on June 06, 2018 at 16:30Hello  stI try to use stm32f746 nucleo  as slave controller with raspberry pi3  I use spi as communication method for metal bare code there is no any problem but when I put code in a thread for communication then I fa...

egywell by Associate II
  • 620 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L496 I2C1/3 cannot work on GPIOG port.

Posted on April 08, 2018 at 09:13L496 port G includes two I2C- PG13/14 I2C1 and PG7/8 I2C3. But the two I2C cannot output and the oscilloscope does not display waveform.I2C1/I2C3 can work correctly if they are mapped to other ports. So I think the I...

ray by Associate II
  • 2858 Views
  • 5 replies
  • 0 kudos

Resolved! Any examples with f_findfirst/f_findnext for 746D?

Posted on June 05, 2018 at 17:23ST seems to do reading all files in a directory in a hard way.I am combining two examples about Sdfat but ST uses unfamiliar commands for reading all files in a directory. I think I could do it with a hard way but isn...

LMI2 by Lead
  • 4846 Views
  • 11 replies
  • 0 kudos

Resolved! Program stm8 with stm32 nucleo board

Posted on June 06, 2018 at 12:09Hello,I would like to know if it is possible to program a stm8 MCU with the stlink of stm32 nucleo board (NUCLEO-L073).Regards,Aurélien

Flash programming alignment error on Nucleo-L4R5ZI

Posted on March 07, 2018 at 01:28Hello, when trying to flash a Nucleo-L4R5ZI through Atollic TrueStudio 9.0.0 on a most recent Debian stable, I keep getting the error below.I am using STLink Firmware V2J30M19 (newest). Does anybody have an idea? Tha...