cancel
Showing results for 
Search instead for 
Did you mean: 

DMA irqHandler doesn't work

Damiano Balzani
Associate III
Posted on February 15, 2018 at 11:25

Hi everyone,

I'm tryng to use DMA with ADC on STM32L051x6 MCU.

When i see the Memory dump at the memory address of variable i takes the correct value from ADC DR but DMAIrq doesn't work never

Can somebody help me?

Thanks in advance

bool LED_CURRENT_ADC_Init(void)

{

   LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1); //Enable DMA Clock

   DMA1_CSELR -> CSELR &= 0xFFFFFFF0; //Remap of DMA channels to ADC

   LL_ADC_REG_SetDMATransfer(ADC1, LL_ADC_REG_DMA_TRANSFER_UNLIMITED); //Enable DMA    transfer on ADC

   DMA1_Channel1 -> CPAR = (uint32_t) (&(ADC1->DR)); //Configure the ADC data register address

   DMA1_Channel1->CMAR = (uint32_t)(ADC_val); //Configure the memory address

   DMA1_Channel1->CNDTR = 1; //Configure the number of DMA tranfer to be performs on channel 1

   LL_DMA_SetChannelPriorityLevel (DMA1, LL_DMA_CHANNEL_1, LL_DMA_PRIORITY_VERYHIGH); 

   LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_1, LL_DMA_MODE_CIRCULAR); //Set mode    LL_DMA_MODE_NORMAL LL_DMA_MODE_CIRCULAR

   LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_1,    LL_DMA_DIRECTION_PERIPH_TO_MEMORY); //Set direction

   LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_1, LL_DMA_MDATAALIGN_WORD); //Set dimension

   LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_1, LL_DMA_MEMORY_INCREMENT); 

   LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_1, LL_DMA_PERIPH_NOINCREMENT); 

   LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_1, LL_DMA_PDATAALIGN_HALFWORD); 

   LL_DMA_EnableIT_TC(DMA1, LL_DMA_CHANNEL_1);

   LL_DMA_EnableIT_TE(DMA1, LL_DMA_CHANNEL_1);

   LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_1);

   NVIC_EnableIRQ(DMA1_Channel1_IRQn);

   NVIC_SetPriority(DMA1_Channel1_IRQn, 1);

LL_ADC_SetClock(ADC1, LL_ADC_CLOCK_SYNC_PCLK_DIV1);

LL_ADC_SetSamplingTimeCommonChannels(ADC1, LL_ADC_SAMPLINGTIME_7CYCLES_5);

LL_ADC_SetResolution(ADC1, LL_ADC_RESOLUTION_12B);

LL_ADC_SetDataAlignment(ADC1, LL_ADC_DATA_ALIGN_RIGHT);

LL_ADC_REG_SetSequencerChannels(ADC1, LL_ADC_CHANNEL_3);

LL_ADC_REG_SetContinuousMode(ADC1, LL_ADC_REG_CONV_SINGLE); //LL_ADC_REG_CONV_SINGLE LL_ADC_REG_CONV_CONTINUOUS

LL_ADC_ClearFlag_ADRDY(ADC1);

LL_ADC_EnableIT_EOS(ADC1);

LL_ADC_Enable(ADC1);

while(!LL_ADC_IsActiveFlag_ADRDY(ADC1))

{

}

return true;

}

#dma-adc
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on February 15, 2018 at 14:00

The DMA Irq will not occur if the DMA transfers aren't actually occurring. Check the DMA for error flags.

Check the handler name matches the one in the vector table, and the linker binds correctly.

Don't see the array defined. Check WORD != HALFWORD

Perhaps the are some L0 LL examples you can review.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2
Posted on February 15, 2018 at 14:00

The DMA Irq will not occur if the DMA transfers aren't actually occurring. Check the DMA for error flags.

Check the handler name matches the one in the vector table, and the linker binds correctly.

Don't see the array defined. Check WORD != HALFWORD

Perhaps the are some L0 LL examples you can review.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Damiano Balzani
Associate III
Posted on February 22, 2018 at 11:06

thanks for the help!