STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Switch Nucleo program from a prototype

Posted on June 06, 2018 at 10:48Hello, I made a model NUCLEO-L053R8 card containing modules X-NUCLEO-IKS01A1 and X-NUCLEO-IDS01A4. Now,I want to switch my program used for the NUCLEO card to another project, that of my prototype which containing a S...

CDC HOST enumeration problem.

Posted on June 06, 2018 at 10:22I have CDC HOST. (stm32f205)It is work normal, but when i connect to this same device(CDC Device (stm32f303 )) i can get a problem with enumeration.  It is if device in resert or not started normaly.  In this case HOS...

reserv70 by Associate II
  • 652 Views
  • 0 replies
  • 0 kudos

I-CUBE-LRWAN v1.1.2

Posted on June 06, 2018 at 07:09From where can I download I-CUBE-LRWAN v1.1.2? The current version is 1.1.5 but I need v1.1.2

I want to get data about hands-on workshop from st.

Posted on December 06, 2016 at 01:14Excuse me.I want to get data about STM32 hands-on workshop.(such as presentation file, pdf, sample codes)I don't attend off-line hands-on workshop.So, I want to see a relevant data about hands-on workshop.Let me k...

STM32H7 - SDMMC not working

Posted on February 13, 2018 at 13:22HiI'm having quite an issue while using the FatFs on a SD card.I configure everything on the Cube following this tutorial :https://www.youtube.com/watch?v=kRhF44v2ezM  I'm kinda lost, and i would like some support...

HAL API to format the contents of a SD card

Posted on June 06, 2018 at 07:41I have a 32 gb sd card. I have interfaced it with STM32F407 Discovery board with 1 bit SDIO through Cubemx. When i use a formatted SD card i am able to write files into the card. Now, i want to format the card using s...

SPI_EEPROM_M95640R

Posted on June 01, 2018 at 05:07Hello all,I'm here using the M95640 EEPROM and communicating via SPI. It looks like I'm sending all the signals correctly from my MCU side, but the device (M95640) is not responding to Signals.Below is the WriteEnable...

0690X0000060Kz3QAE.png 0690X0000060KvjQAE.png 0690X0000060KrJQAU.png