STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Calling HAL_Delay while in sleep

Posted on July 03, 2018 at 05:23Hi,What is the expected MCU power consumption / CPU state when calling HAL_Delay() from an ISR triggered while MCU is in STOP mode? 

STM32CubeMX H743ZIT Makefile problems

Posted on July 03, 2018 at 00:08I'm trying to build a simple 'hello world' program on the STM32H743 using the Makefile option and the standard Ubuntu arm-none-eabi-gcc V 4.9.3.  At this stage my program doesn't even do floating point, but it will ev...

Difficulties with the purchase of sdtam 16Mx32 512Mbit.

Posted on July 02, 2018 at 12:53At the moment, almost all the memory chips of such a configuration are discontinued. They were not popular at the time of active sales, and after the end of support for manufacturers - leftovers remained at an inadequ...

STM32F767 External SRAM

Posted on June 30, 2018 at 18:33Hi .I have a custom board with ''stm32f767'' mcu on it and an external sram ''is62wv51216bll-55tli ''.I have two problem first is when MPU is Disable and i have this config :↓  SCB_EnableICache();  SCB_EnableDCache();...

0690X0000060LYpQAM.png
M N by Associate II
  • 3785 Views
  • 10 replies
  • 0 kudos

Set WKUP pin to no push/pull after Standby STM32

Posted on June 25, 2018 at 17:14When I send the device into standby it appears that the WKUP pin is held low. For my application this causes an issue with the Comparator that is in the circuit before the pin. Is there a way to configure the WKUP pin...

STM32L0: wrong address of COMP registers in svd file

Posted on July 02, 2018 at 13:33Hello! I use MDK from Keil and noticed, that the address of the COMPn_CSR registers in the SystemViewer have wrong addresses.I checked the SVD files in the latest STM32L0xx_DFP V2.0.0. The problem is the base address ...

SD CARD STM32L052

Posted on June 22, 2018 at 13:51Hi everybodyI have little trouble about STM32L052 and SD Card reader.I don't have much knowledge about SPI communication in STM and I never used before SPI,FATFS but it seems to complex to me  anyone can help me ? If ...