cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F031C6T forward compatible to F051, F071 and F091

gerald23
Associate II
Posted on March 09, 2018 at 16:21

We are working on a motor controller and started with a evaluation board that uses the STM32F031. Unfortunately we have utilized over 80% of the flash and 90% of the RAM, so going forward with the STM32F031 is a bit risky. Rumor has that some of the STM32 series parts are forward compatible.

What about the F031?

Will it port to upward?

Is there any limitations?

#compatible #port-upward #stm32f031c6t
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on March 09, 2018 at 17:45

Not sure why you'd need to rely on rumors, the documentation, libraries and tools are openly available for review. Your FAE should be able to provide specific advice.

Pin-for-pin compatibility works until it doesn't, ie parts on the market, with data sheets, will be what they are, future products or families might not be, and be inconveniently different while still being touted as 'pin-for-pin'. Do your due diligence. If the Design Manual says make specific accommodations in your design and PCB layout, and power routing, PAY ATTENTION, even if the reasons aren't fully explained, these provide the wiggle room you'll need later to account for differences in future offerings.

I've not had much problems migrating across assorted STM32 parts spanning a decade, I understand how to port software, I understand how to partition my software.

The pin muxing options on new STM32 parts have gotten better, but they don't provide a lot of maneuverability, and frequently choices seem to have been made while being trapped in a conference room with dropping oxygen levels.

Pick parts with more pins, low pin count devices are going to limit your choices (availability, range, pin escape), and options with larger die sizes,  advanced parts are more likely to be in packages with 64 to 100 pins.

If you keep expanding the code size are you going to run out of speed to run all of it? Beyond 24 MHz the CM0(+) designs here typically scale very poorly due to inherent slowness of the FLASH and lack of mitigating cache/logic. ie a part running a 48MHz isn't anywhere close to 2x one running at 24MHz

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
T J
Lead
Posted on March 10, 2018 at 07:02

I use the '091 now,  256k / 32k ram

its a great chip, close to $2

its likely to very close to drop in replacement anyway,

did you make your own board?

you may need some slight adjustment..

easiest way to check is firstly the pinout diagrams,

ie check 'F031  Vs 'F091    LQFP100 pinout , (which ever formfactor you have)

then check the peripheral options in the datasheet ie checking PA6 on F031 Vs F091 

I think you will be surprised how close it is.