STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

f_mount always returning FR_NO_FILESYSTEM

Posted on July 12, 2018 at 11:39I am using system workbench (eclipse) as IDE and cubemx to provide setup code for both SDIO(1 bit mode) and FATFS middleware. I am using a STMF407VE and have double checked the SD adapter has correct pin-out.FATFS myf...

STM32F4 eMMC CMD signal voltage levels

Posted on July 12, 2018 at 22:23I'm developing a system that uses an STM32F4 with an eMMC from Micron.  The issue I'm having is related to the voltage levels I'm seeing on the CMD line.  When the STM32 is driving the line I see good 3.3V levels.  Ho...

shannon2 by Associate II
  • 3938 Views
  • 4 replies
  • 0 kudos

Firmware Over the Air(FOTA)

Posted on July 13, 2018 at 14:11Hello EveryOne ,                              I am using STM32L432KB controller with GSM connectivity within it and need to develop the code to update the firmware in controller(for remote controllers). But I am confu...

K_P_D by Associate II
  • 1840 Views
  • 1 replies
  • 0 kudos

BSP libraries and pin configuration

Posted on July 13, 2018 at 11:50I'm using BSP libraries for STM32F469I-Discovery board. This board has goldpin female connectors matching Arduino Uno, so that Arduino shields may be used. Since BSP libraries have their own HAL configuration, do they...

Usart3 communication with st link

Posted on July 04, 2018 at 09:59I have implemented usart in stm32f746 series ,i'm using usart3 pd8 and pd9 port but it is not sending any data to serial port (putty im using),my doubt is should i connect  usb to ttl conveter to these particular pins...

mani s by Associate III
  • 1883 Views
  • 5 replies
  • 0 kudos

is PWR_CR register available on category 3?

Posted on July 12, 2018 at 18:31Hi everyone,i'm trying to set the ULP bit in PWR_CR register. I'm using a 3 category device.Is it possible? i'm not able to understand if it is possible or notCan you help me?Thanks in advanceDamiano

TIMx_CH1_ETR vs TIMx_CH1

Posted on July 12, 2018 at 14:55Could you explain me the difference between TIMx_CH1_ETR and TIMx_CH1, please?In deed, I would like to replace STM32L071 with STM32F091 (PA0 - pin n°14).In general, I would like to connect an external clock to a timer...

moez0102 by Associate II
  • 1958 Views
  • 2 replies
  • 0 kudos

HAL_CAN_transmit_issue

Posted on September 08, 2017 at 14:05Hi, I am using StM32f042f4 (20 pin) for my project. I am getting stuck in can transmit. Logic work fine with different m0 controller. How can i solve it ? How do i check the error? #include 'main.h'#include 'stm3...

Error word in RM0008: STM32F10x data for DAC channel2 to be loaded into DAC_DHR12LD [27:16] bits. What is correct DAC_DHR12LD[27:16] or DAC_DHR12RD[27:16]?

Posted on July 13, 2018 at 10:29STM32F10x DAC (stm32f_ref Manual_RM0008, page248)........data for DAC channel2 to be loaded into DAC_DHR12LD [27:16] bits.What is correct DAC_DHR12LD[27:16] or DAC_DHR12RD[27:16]?? error wordI think  Right about  DAC_...

csocom by Associate II
  • 1139 Views
  • 2 replies
  • 0 kudos