STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDMMC Data Timeout Error

Posted on April 30, 2018 at 18:19HiI'm trying to write some test data to SD card by DMA with Nucleo-F767Zi.Every 100ms I write 20 blocks to SD card by calling the HAL_SD_WriteBlocks_DMA() method.I have a counter to record how many times the HAL_SD_W...

New forum lacking return links

When I make a post, I have to click at least three links to get back here. Hitting the back button only brings me to some sort of "ping timeout" page. Please either increase the timeout, or provide links back to the top. Links back to anywhere fro...

STM32L4A6VGT power consumption?

Hi,I am measuring a STM32L4A6VGT board power consumption. From the datasheet, in standby mode should be 120nA while I got the value @ 19 mA (last Friday). The FW does nothing, in main after MX_XXX init, call HAL_PWR_EnterSTANDBYMode(). Now I am gett...

STM32 FatFS SDIO DMA bug

Posted on June 14, 2018 at 23:28How to reproduce:1) Use STM32Cube FW_F4 V1.21.0 (not tested on other versions)2) Set up SDIO 1-bit mode with default parameters.3)4) Set up FatFS with SDIO driver with default parameters.5) Set 'Use dma template'=enab...

STM32F427 and SDRAM

Hi guys,I'm using an stm32f427 interfaced with an external SDRAM by mean of FMC controller.The controller is configured with SDRAM clock period = 2 x HCLK periods and to support burst read (RBURST bit = 1).It's not clear to me how to set the RPIPE pa...

Bucky by Associate II
  • 1405 Views
  • 1 replies
  • 0 kudos

Reset and hold counter value on low level

Dear communityI am trying to make a timer/counter reset it's counter value on a falling edge and then hold the value until a rising edge (see attached ​picture for illustration). I am at the moment working on a L152, but I might soon be working on a ...

KMoge by Associate
  • 1417 Views
  • 1 replies
  • 0 kudos

X-CUBE-IAP-USART problem

Hello, I'm trying to use example code provided by X-CUBE-IAP-USART package to develop IAP FW for STM32L0xx device. I'm using STM32L073 Nucleo64 board for development.When I send compiled FW using TeraTerm's YMODEM protocol nothing happens. Only thing...