cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L0 I2C: Is NBYTES[7:0] latched upon START condition and can not be changed until TCR flag is high?

Pieter Conradie
Associate III
Posted on April 06, 2018 at 16:02

Hi everyone,

I'm trying to create my own blocking I2C driver and want to split the usage up into a few primitive functions, e.g. for I2C Master Transmitter, the following functions apply:

bool i2c_start_write(uint8_t sla_adr);

bool i2c_wr_u8(uint8_t data);

bool i2c_stop(px_i2c_handle_t * handle);

In i2c_start_write() I do the following:

1. Wait until I2C_ISR_BUSY=0

2. I2C_CR2_SADD = sla_adr

3. I2C_CR2_RD_WRN = 0

4. I2C_CR2_RELOAD = 1

5. I2C_CR2_NBYTES = 0 (I do not know yet how many bytes will be needed to be transmitted)

6. I2C_CR2_START = 1 (to generate START condition and SLA+W)

7. Wait until I2C_CR2_START = 0

8. Check I2C_ISR_NACKF to verify that I2C slave ACK'd

In i2c_wr_u8() I do the following:

9. Check that I2C_ISR_BUSY=1

10. I2C_CR2_NBYTES = 1 (I want to transmit one byte)

11. Wait until I2C_ISR_TCR is set (??)

12. TXDR = data (??)

13. Wait until I2C_ISR_TCR  is set(??)

At step 10 I can change I2C_CR2_NBYTES, but the I2C peripheral does not pick up this change and start the transmission sequence. Is there a way to 'kick-start' the RELOAD process?

Am I forced to load NBYTES before I begin the START condition?

Thanks in advance,

Pieter

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0