STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

One pulse mode

Hello everyone.I'm studying in stm32f40g eval and using timer in one pulse mode.First I'm use the example code TIM_OnePulse and modify it. I'm add the One pulse OUTPUT in function TIM_Config and One pulse EXTERNAL TRIGGER in function TIM_T2IConfig. I...

How migrate STM32L432KC MCU to STM32L452RE MCU?

How can we provide support to two devices (startup files) for a developed application. I am using STM32L432KC MCU and i want to migrate my application to STM32L452RE MCU. Is there any way to do the same?

Niks by Associate II
  • 1302 Views
  • 2 replies
  • 0 kudos

Resolved! STM32f746G - Discovery - Audio Pins

Hi I am having issues with playing sound through the audio out jack. I have gone through the BSP examples but what's lacking for me is the correct setup of the pins. At the moment I have set up -SAI2 Block A (Master) - (I2S/PCM enabled)I2C3 I2S3 DMA ...

Avan.7 by Associate II
  • 1184 Views
  • 1 replies
  • 0 kudos

Resolved! Complementary outputs with dead-time?

Hello,I'm trying to have complementary outputs with dead-time on CH1/CH2/CH3 and CH1/CH2/CH3N using TIM1 and Output Compare Mode on STM32F429.So I configured STM32CubeMX like in the picture below :And there is the portion of my code :(for testing pur...

0690X000006BskZQAS.png 0690X000006BskUQAS.png

Resolved! How to correctly initialize and config SVC interrrupt

I'm creating a context switch program for a personal mini ARM kernel project and the context switch program is written entirely in Assembly. The problem is when I make a SVC call (svc 0) I enter the SVC_Handler but when I try to execute the next inst...

SMola by Associate II
  • 4878 Views
  • 6 replies
  • 1 kudos

STM32L4A6RG Jumping to application address

Posted on August 28, 2017 at 08:46I divided internal Flash to two part as below:1. bootloader start address: 0x08000000 (size: 0x8000)2. application start address: 0x08008000Now,I'm using the following code in bootloader to jump to application, it's...

IAP Procedure doesn't work - strange behavoiur

Hello everyoneI'm using STM32F072 microcontroller. I've to update my software reading from an external memory via SPI the whole HEX program, and the program it in the flash. To do so, I do the steps:Create a section in the linker file called ramfuncS...

0690X000006BsXaQAK.png