DFU USB disabling.
Please tell me how to disable the DFU USB in application code.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Please tell me how to disable the DFU USB in application code.
How to disable the low power mode of stm32l072 controller.
I've got a few problems when creating a simple project using STM32CubeMX :1) using all the default setting by STM32CubeMX and clicked YES to "initialize all peripherals with their default MODE", the LED ports were default to input mode ! Weird ! If s...
jtag status contains invalid mode value - communication failure
static void MX_UART4_Init(void) { huart4.Instance = UART4; huart4.Init.BaudRate = 9600; huart4.Init.WordLength = UART_WORDLENGTH_8B; huart4.Init.StopBits = UART_STOPBITS_1; huart4.Init.Parity = UART_PARITY_NONE; huart4.Init.Mode = UART_...
Hello after installing the latest version of CUBEMX(4.27) and generating a default project for my STM32F411VE Discovery board by choosing the option to initialize all the peripherals in their default mode it ended up not working. After some debugging...
when i configured my stm32 board as master then i transmit data but in slave mode it does not..i even tested the i2c example provided by Cube MX ,there also i can only transmit data in master mode,but not in slave mode...any idea please?