2018-06-19 7:39 AM
Dear Sir/Madam:
I am using STM32F4x nucleo HAL lib, and try to set timer interrupt. It does not work. Here are the settings for timer interrupt:
..... // Timer is configured to be triggered every .05 secs.
__TIM4_CLK_ENABLE();
Tim4Handle.Init.Prescaler = 16400;
Tim4Handle.Init.CounterMode = TIM_COUNTERMODE_UP;
Tim4Handle.Init.Period = 20;
Tim4Handle.Instance = TIM4;
Tim4Handle.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
if ( HAL_TIM_Base_Init(&Tim4Handle) != HAL_OK )
{
Error_Handler(); }
TIM_SlaveConfigTypeDef sSlaveConfig;
TIM_MasterConfigTypeDef sMasterConfig;
sSlaveConfig.SlaveMode = TIM_SLAVEMODE_RESET;
sSlaveConfig.InputTrigger = TIM_TS_ITR0;
if (HAL_TIM_SlaveConfigSynchronization(&Tim4Handle, &sSlaveConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&Tim4Handle, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
HAL_TIM_Base_Start_IT(&Tim4Handle);
HAL_NVIC_SetPriority(TIM4_IRQn, 0, 1);
HAL_NVIC_EnableIRQ(TIM4_IRQn); .....
here is my interrupt routine(it is never got called):
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
// send gpio signal to scope
}
would you please help me to see any problem?
thanks roseanne
#stm32f4-nucleo #initialization-timer-hal #stm32l4-hal-timer #stm-mcu #timer-interruptsSolved! Go to Solution.
2018-06-19 11:40 AM
>>Do I need to use
TIM4_IRQHandler()
to call HAL?
Yes, otherwise how will the plumbing work?
/**
* @brief This function handles TIM interrupt request. * @param None * @retval None */void TIM4_IRQHandler(void){ HAL_TIM_IRQHandler(&Tim4Handle);}
There is a lot of example code covering multiple boards, and portable
STM32Cube_FW_F4_V1.21.0\Projects\STM32F401-Discovery\Examples\TIM\TIM_TimeBase\Src
2018-06-19 8:34 AM
Seems to be a lot of unnecessary code just to set up a time-base.
What frequency are you running the part at?
Make sure the Init structure is clear/clean.
Review Prescaler and Period settings, these should be in the N-1 form, ie for N counts 0 thru N-1, the values describe the limit.
..... // Timer is configured to be triggered every .05 secs (20 Hz)
/* TIM handle declaration - global */
TIM_HandleTypeDef Tim4Handle = {0};__TIM4_CLK_ENABLE();
Tim4Handle.Init.Prescaler = 8400 - 1;// APB1 @ 42 MHz, TIMCLK @ 84 MHz
Tim4Handle.Init.CounterMode = TIM_COUNTERMODE_UP;
Tim4Handle.Init.Period = 5000 - 1; // 100KHz to 20Hz
Tim4Handle.Instance = TIM4;
Tim4Handle.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
if ( HAL_TIM_Base_Init(&Tim4Handle) != HAL_OK )
{
Error_Handler();
}HAL_TIM_Base_Start_IT(&Tim4Handle);HAL_NVIC_SetPriority(TIM4_IRQn, 0, 1);
HAL_NVIC_EnableIRQ(TIM4_IRQn); .....
And you have a TIM4_IRQHandler() calling into the HAL?
2018-06-19 11:02 AM
Dear Sir:
thanks for your quick response!
About your last question, :
you have a TIM4_IRQHandler() calling into the HAL?
in my understand to HAL lib, I only need to define :
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
// send gpio signal to scope
}
which will be called once interrupt happen.
Do I need to use
TIM4_IRQHandler()
to call HAL? if so, How could I do that?
thanks
ro
2018-06-19 11:40 AM
>>Do I need to use
TIM4_IRQHandler()
to call HAL?
Yes, otherwise how will the plumbing work?
/**
* @brief This function handles TIM interrupt request. * @param None * @retval None */void TIM4_IRQHandler(void){ HAL_TIM_IRQHandler(&Tim4Handle);}
There is a lot of example code covering multiple boards, and portable
STM32Cube_FW_F4_V1.21.0\Projects\STM32F401-Discovery\Examples\TIM\TIM_TimeBase\Src
2018-06-19 12:15 PM
Dear Clive:
thanks for your help!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
after I add it, both uart and timer interrupt all work!!!!!!!!!!!!!!!!!!!!!
thanks
rose
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.