STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Overrun when using the DMA

Hi,I've run into an interesting problem when doing two simultaneous SPI transfers using the DMA.I'm using the STM32F103ZFH6 where I am simultaneously reading a bitstream (in large chunks) from and external SPI flash device and writing in out to anoth...

SK by Associate
  • 5631 Views
  • 6 replies
  • 0 kudos

ADC configuration of STM32F051 controller

Can i configure three different ADC channels using ADC interrupt.If so yes, how can i read my values corresponding to each channel from ADC ISR?I have configured ADC interrupt in such a way that the interrupt triggers after all channel sequence.(Havi...

Amal Babu by Associate III
  • 1460 Views
  • 2 replies
  • 0 kudos

can't enter stop mode when connect an emluator

when there's no emluator connected, my program works ok. But when I have my emluator connected, my program will immediately recover from stop mode or may even not enter into stop mode?  ​Do somebody has same experience and give me some ideas?​

xleij by Associate II
  • 1100 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L4 -Analog WatchDog with Interrupt in HAL library

I am using STM32L432 with HAL library. I am programming ADC1 Channel 16 (i.e. PB1) as analog input signal. I have initialized ADC as Analog WatchDog-1 with Interrupt and without DMA, so that I dont have to continuously monitor my input voltage, if my...

Trouble with 16 bit DMA transfer memory to peripheral

Hello,I have a strange problem with a 16 bit DMA transfer memory to peripheral on STM32F439, using Nucleo F439ZI.My goal is to create a sequence of pulses with different pulse widths. I use a timer (TIM2), set its prescaler and set Ch1 to toggle on m...

DCMI bitdepth of STM32H7 for Raw Bayer data

Posted on March 31, 2018 at 18:03Can a STM32H7 capture 12-bits raw bayer progressive video data? For instance, from an OV5642 image sensor?I'm looking at the reference manual of the MCU. It can be found from the following link.http://www.st.com/cont...

M. Jeong by Associate II
  • 3559 Views
  • 7 replies
  • 0 kudos