Skip to main content
Jim Seymour
Senior
June 21, 2018
Question

Possible bug found in HAL_CAN_IRQHandler (STM32Cube FW_F0 V1.9.0)

  • June 21, 2018
  • 1 reply
  • 613 views
Posted on June 22, 2018 at 00:29

I have struggled over the last couple of weeks to implement an interrupt-driven CAN system on a STM32F042K6 using CubeMX v4.26.0 and FW_F0 V1.9.0.

Now that I finally have it working, I found what I believe is a bug in HAL_CAN_IRQHandler() - and thought others might be interested.

At line 1384 in stm32f0xx_hal_can.c, there is a call to __HAL_CAN_DISABLE_IT() to disable a bunch of interrupts when an error is detected.  Included in these are CAN_IT_FMP0 and _FMP1 - which are required to receive messages.

HAL_CAN_Receive_IT() properly enables the relevant FMPx interrupt.  But then if there's some kind of glitch on the bus and ANY error interrupt occurs, FMPx will be cleared.  A message that arrives after this glitch will not generate an interrupt and will be ignored.

While I've used a variety of STM32 chips in various projects, this is my first foray into CAN on the STM32, so feel free to correct me if I'm wrong!

Workaround: Enable HAL_CAN_ErrorCallback() as follows:

void HAL_CAN_ErrorCallback(CAN_HandleTypeDef *canp) {

// Re-enable receive interrupts!

// (The error handling code in HAL_CAN_IRQHandler() disables this for some reason!)

__HAL_CAN_ENABLE_IT(canp, CAN_IT_FMP0 | 

CAN_IT_FMP1);

// (or only re-enable the one you are using)

}

Alternate (uglier) workaround: Use a polled system for CAN receives.

Real fix: In stm32f0xx_hal_can.c, do not disable ALL the interrupts when an error is detected.  It seems like it should only disable the error interrupts - as follows:

/* Disable interrupts: */

/* - Disable Error warning Interrupt */

/* - Disable Error passive Interrupt */

/* - Disable Bus-off Interrupt */

/* - Disable Last error code Interrupt */

/* - Disable Error Interrupt */

__HAL_CAN_DISABLE_IT(hcan, CAN_IT_EWG |

CAN_IT_EPV |

CAN_IT_BOF |

CAN_IT_LEC |

CAN_IT_ERR);

Thanks.

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    June 22, 2018
    Posted on June 22, 2018 at 11:14

    Hello

    Seymour.Jim

    ,

    I will raise this issue internally for check.

    With Regards,

    Imen.

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks