User Activity

Hi everyone. I'm using MotionGC library to calibrate my LSM6DSL gyroscope. In User Manual of library it is stated that "void MotionGC_Initialize(float freq) "function takes "float" as input argument. But when I call the function according to the us...
Hi everyone. I'm new to motor control and have some problems with my robot. We are designing a three-wheeled omnidirectional robot which should bare and transport weights about 10 kg. We use Pololu 12V DC motors which has a stall torque of 8.5kg-cm....
Hi everyone, i'm working on a project which i use Atollic TrueStudio as IDE and NUCLEO-F303RE as evaluation board. I was inplementing floating point as "hardware" before i decided to use MotionAC library but after adding library to my project i could...
Hi everyone, i've just started to learn using MEMS libraries in my project and have some questions. First of all; my device is a three wheeled omniwheel-omnidirectional robot which can move only on a flat table(i.e. XY-plane only). So no movements in...
Hi everyone, i have a clear internet connection and i can browse all websites properly. But my STM32CubeIDE can not connect internet in order to download firmwares necessary to create project. How can i solve this issue.Thanks.
Kudos from