STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Glitch free duty cycle update

Hi, I am trying to update the duty cycle output on a STM32F107 MCU, glitch free of course. I know I have to set the appropriate PE bit in the TIMx->CCMRx register. This can be done with the library function TIM_OCxPreloadConfig(). At the time I make...

EGrom by Associate II
  • 2576 Views
  • 6 replies
  • 0 kudos

Why ADC watchdog is not triggering.

The code is as follows.... RCC_AHBPeriphClockCmd (RCC_AHBPeriph_DMA1, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);...

0690X000006CFSmQAO.jpg
SConf by Associate II
  • 941 Views
  • 1 replies
  • 0 kudos

DMA STM32L0 operation

Hello. I am using STM32L053R8T6. I connect 3 ADC channels (PA4, PA6, PA7). For this I use DMA. I need the resolution of the ADC - 8 bits, for this I initialize an array with the dimension of 8 bits (volatile uint8_t AdcValue [3];)I am using DMA HAL_A...

0690X000006CFEfQAO.png
ABoga by Associate
  • 928 Views
  • 1 replies
  • 0 kudos

HardFault exception problem

I make boot loader for jump to 0x08020000And, I make program that start from 0x08020000, also same vector table address(0x08020000)It works well, but sometimes(when program modified), it doesn't workI use debugger, and get result below//Fault excepti...

0690X000006CFCoQAO.jpg
mcho.19 by Associate II
  • 5393 Views
  • 8 replies
  • 0 kudos

STM32F446RE I2S can't output clock

hi all, I wan to use PA4, PA5 and PA7 as I2S.but can't output clk. follow is code for I2S setting: // clock setting   RCC_PLLI2SConfig(16, 334, 2, 7, 7);  RCC_I2SCLKConfig(RCC_I2SBus_APB1, RCC_I2SCLKSource_PLLI2S);  //RCC_I2SCLKConfig(RCC_I2SBus_APB2...

khuan.81 by Associate
  • 2171 Views
  • 6 replies
  • 0 kudos

Is it possible to configure the IWDG timer to 30 minutes?

I have an IoT hardware (using STM32L152) that carry out some tasks and go to STOP mode for 30 minutes. Then, it will wake up and repeat the same process again. Now, I would like to add the watchdog timer to ensure everything works fine. My question i...

Khoo.B by Associate III
  • 2588 Views
  • 5 replies
  • 0 kudos