STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

various defines stop working from includes

OK, I'm going crazy. stm32f4xx_hal_def.h is included in just about every file. Defined in this header is Hal_StatusTypeDef - Not found when compiled. I made no changes that could have impacted this. Prior to Hal_StatusTypeDef not being found, I ha...

Failure on STM32L4 SPI receive

Hello All,I have an STM32L486 and use the SPI3 to connect a SPI flash device.The code uses CubeMX L4 1.13 HAL SPI and seems to work.But after reflash or reboot the SPI returns only 00h values.After an power on reboot it looks all fine.I compared in t...

taraben by Senior
  • 1287 Views
  • 4 replies
  • 0 kudos

Time-stamp by chaining two STM32 timers.

Hello Everyone,I have a requirement to track time and generate timestamps when an event occurs. I have tried time_base, input capture methods and trying with chaining two timers now.I wanted to know if it is possible to chain 2 timers in STM32L0 and ...

Interfacing stm32f1 with GSM

I am trying to interface GSM with my ARM controller [stm32f103c8t6].I knew a little about the working of GSM, - By sending the "AT" command to GSM, it will respond with a "OK" message.Before interfacing GSM with arm, i learned how to use HAL_uart fun...

0690X000006CSvSQAW.jpg
Bud by Associate III
  • 2852 Views
  • 1 replies
  • 0 kudos