User Activity

Posted on July 04, 2018 at 11:07Hello,i'm using a STM32L475VCT with STM32CubeMx 4.26I use the TIM17 with Break function. In CubeMx break filter is possible but not in the reference manual RM0351 Rev. 6 page 1157.ThanksPhilippe
Posted on July 04, 2018 at 10:54Hello,i'm using a STM32L475VCT with STM32CubeMx 4.26I need to use the COMP2 with blanking function. I configured the TIM8 OC5 in CubeMx but when i read the datasheet, the only blanking source is the TIM15 OC1. The doc...
Posted on June 07, 2018 at 09:32Hello,i have updated STM32CubeMx from 4.25.1 to 4.26 and now i can no more generate my project. It freezes during the generation project. I uses a STM32L475.ST, please give me a link to download the 4.25.1 version bec...
Posted on August 25, 2017 at 11:12Hi,i'm using the a STEVAL-IHM034V2 board for evaluation (PFC + FOC PMSM).I imported the project in ST Workbench 4.3. Generated files and compiled with IAR is OK. Then board is programmed.The motor starts but the PFC...
Posted on December 02, 2016 at 10:11Hello,I'm using a STM32F334 and when i updated cube Mx from 4.17 to 4.18 i had no more possibility to configure the trigger source for the ADC 2. It's impossible to find the 4.17 for downloading again. Why ST does...