User Activity

Project imported: D:\Vrund\STM32CubeExpansion_SBSFU_V2.4.0\Projects\STM32F413H-Discovery\Applications\1_ImageIssue faced:15:42:35 **** Build of configuration Debug for project STM32F413H_DISCOVERY_1_Image_SECoreBin ****make all Building file: D:/Vrun...
Hello,I want to use sbsfu for STM32L562 controller with STM32Cube IDE version 1.5.AS per primary research i am using below package and project .I am using STM32SecuWS package.Under that project I am using is STM32SecuWS\TFM\STM32Cube_FW_L5_V1.3.0\Pr...
Hello,I have imported existing project to cubt ide version 1.5.below is the problem i am facing.Problem running CDT Scanner Discovery provider com.st.stm32cube.ide.mcu.toolchain.armnone.setup.CrossBuiltinSpecsDetectorError serializing language settin...
I have signature of my user app and user app in .bin format.if i have to use only these two inputs, what modification i need to do in SBSFU? and under what files?i dont want to use post built .bat and prebuilt.bat.i am using Single slot image example...
I am working on ethernet bootloader through TFTP for stm32f407.If i use available ethernet bootloader from ST site which do not use HAL library, it works perfect.If i generate code using stm32 cubemx which uses hal library, (tftp file is taken same a...