Question
How can I increase the ADC sampling frequency up to 2 MHZ?
I have only been able to increase it up to 600 KHz. I have studied the speed the ADC peripheral should have and should be even higher, it can be set at up to 84 MHz, with a prescaler of 2 and 6 bits of conversion should be 9 cycle clocks, resulting this on 4 MHz, but it is still acquiring at 600 KHz. What can be wrong?