STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What‘s the actual GBW of OPAMP in STM32F303?

(yellow line: non inverting inputblue line: output of OPAMP )Hi,I am using the NUCLEO-F303RE board and now I am testing the OPAMP3 , which is one of the peripherals in STM32F303. I have set the PA1 as non inverting input, PB2 as inverting input. And...

0690X000006CTW4QAO.bmp
KMak by Associate
  • 997 Views
  • 1 replies
  • 1 kudos

SPI frame longer than 16 bits with stm32f103

Hi,I need to perform write and read operations on an external flash memory through spi protocol.The spi peripheral in the stm32f103 can be configured to 8 or 16 bits data frame lenght. I would like to be able to send longer frames. Is it a possible s...

abcdef by Associate
  • 843 Views
  • 0 replies
  • 0 kudos

Hardfault on IAP jump to APP

Hi guys,I have use the stm32f105 to do a job on the IAP jump tp APP, and normally it works fine, but latest day, I have to disable the USB code on the APP code, then use the flash download demonstrator to download the APP, it runs OK, and then re-pow...

cable gu by Associate II
  • 5271 Views
  • 10 replies
  • 0 kudos

SW4STM32 variables for AC6 version of openocd

I've run SW4STM32 for the last 2 years with an external openocd package but I see that the AC6 version has recently been updated so I thought I'd try it. It gets stored in ~/.p2/pool/plugins/fr.ac6.mcu.externaltools.openocd.linux64_1.21.0.20181113124...

STM32F407 USB FS Device mode Programing

Hi. I am using STM32F407 discovery board programed in USB FS mode. The driver used is WINUSB. mY os IS WINDOWS 10. I am using USF FS configured as ENDP1 OUT and ENDP1 IN. Both in bulk mode. I was managed to successfully enumerated with PC an...

CAN TX ERRORS ??? please help

Hellofollowing the CAN lectures I have a real strange problem transmitting can messageI have two can nodes 1) nucleo 446re board and node 2) is my Can Bus AnalyserI even get the same TX errors in loop back mode & Can normal mode ????why ?? what is wr...

0690X000006CTNWQA4.jpg 0690X000006CTNMQA4.jpg 0690X000006CTNHQA4.jpg 0690X000006CTOPQA4.jpg
JHERI by Senior
  • 1612 Views
  • 0 replies
  • 0 kudos

BOOT0 behavior

Hello!i would like to understand what happens to BOOT0 during the run of regular program (not bootloader).What will happen if i set it to '1' or reset it to '0' during the run?​

YuriCh by Associate II
  • 935 Views
  • 1 replies
  • 0 kudos