Skip to main content
Vitaliy Chernobay
Senior
June 11, 2018
Question

CubeMX 4.25 & 4.26 GRAPHICS configuration MULTIBUF bug

  • June 11, 2018
  • 1 reply
  • 1085 views
Posted on June 12, 2018 at 00:56

If we create a graphics window for GRAPHICS configuration with GUIBuilder for file GUI_App.c

CreateWindow();

The CubeMX is creates function in file STemwin_wrapper.c

void GRAPHICS_Init(void)

{

/* Initialize the GUI */

GUI_Init();

//WM_MULTIBUF_Enable(1);

/* Enable the multi-buffering functionality */

/* Activate the use of memory device feature */

/* USER CODE BEGIN WM_SetCreateFlags */

//WM_SetCreateFlags(WM_CF_MEMDEV);

/* USER CODE END WM_SetCreateFlags */

}

If you delete comments

WM_MULTIBUF_Enable(1);

/* Enable the multi-buffering functionality */

/* Activate the use of memory device feature */

/* USER CODE BEGIN WM_SetCreateFlags */

WM_SetCreateFlags(WM_CF_MEMDEV);

after this, the graphical interface stops running !!!

(Attention!  After deleting comments and compiling, turn off and turn on the power)

The problem is solved by adding a line

WM_MULTIBUF_Enable(1);

/* Enable the multi-buffering functionality */

/* Activate the use of memory device feature */

/* USER CODE BEGIN WM_SetCreateFlags */

HAL_LTDC_ProgramLineEvent(&hltdc, 0); //!!!!!!!!!!!!!!!!!!!!!!!

WM_SetCreateFlags(WM_CF_MEMDEV);

/* USER CODE END WM_SetCreateFlags */

And everything works fine!

P.S.

If FREERTOS is used, it is necessary to eliminate one more bug

that I described before

https://community.st.com/0D50X00009XkXi7SAF

 

in file  ..........STemWin\Target\STemwin_wrapper.c   comment

line (85):

//extern volatile GUI_TIMER_TIME OS_TimeMS;

line (876) :

//   OS_TimeMS++;

#stme32-cube #multibuf
    This topic has been closed for replies.

    1 reply

    Nawres GHARBI
    ST Technical Moderator
    July 4, 2018
    Posted on July 04, 2018 at 11:55

    Hi Vitaliy, 

    Thanks for the report, it will be fixed ASAP (4.26.1 or 4.27.0)