2018-07-03 04:10 AM
In the System Viewer file -> ADC -> ADC1,ADVREGEN is assigned with
[Bit 28]
But as per the below link of reference manual RM0316, it should be
[Bit 29:28]
Thus we request you to provide updated SVD file for this device.
2018-07-04 03:26 AM
Hello
agarwalsankalp1989
,Thank you for bringing this issue to our attention.
This is raised internllay for fix.
With Regards,
Imen