STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I send interrupt command via CDC in STM32?

Posted on February 12, 2018 at 08:18CDC has 3 endpoints (IN, OUT and Interrupt). I have no problem with sending messages via IN and OUT (bulks), but there is a problem when I try use interrupt endpoint (0x82).  I created similar method to USBD_CDC_T...

Timer3 runs 2x faster than expected

Posted on August 04, 2016 at 17:11Timer3 runs 2x faster than expectedI know what many readers are thinking but read onI set my STM32F746 (DISCOVERY PCB) for SysClk=216 MHzAHB Prescaler set to �1 thus HCLK = 216 MHzAPB1 prescaler set to �4 thus PCLK1...

picguy2 by Associate II
  • 4103 Views
  • 6 replies
  • 0 kudos

hi, I have a few stm32f429i discovery old version, they work by USB connection to PC (for power) or by 5v external power supply(without USB connection )

recently I bought some new version (disc1) these start working by connecting USB,but they don't start by 5v external supply without USB connection to PC,I have to connect USB connection to PC and external 5v to proper pin then it starts working , now...

My simple IWDG dont work - why?

Hi.I downloaded some IWDG example code from Keil because I will use the IWDG-feature of my STM32F107. Configurations/init are located in this procedure://__inline static void stm32_IwdgSetup (void) { static void stm32_IwdgSetup (void) {   RCC->...

0690X000006CrtMQAS.png

Resolved! Trouble with ST-LINK/V2 debugger

I'm feeling really stupid about this. We were unable to debug in our circuit, so to check, we have a standalone STM32L021D4Px, mounted to a solderless breadboard. 3.3V is connected to Pin 14, ground to pins 9 and 1, NRST to pin 4, SWDIO to pin 13 and...

Resolved! Problems when reading from FLASH; STM32F4

I successfully write to FLASH but when I try to read I get 0.First I read some data from keyboard to initialize "inter" variable.Then I store it in FLASH, but I can't read it.Here is what I've added to linker .ld file:/* Specify the memory areas */ M...

0690X000006CrQeQAK.png 0690X000006CrQyQAK.png 0690X000006CrRDQA0.png 0690X000006CrT4QAK.png
Jake2451 by Associate
  • 2162 Views
  • 3 replies
  • 0 kudos

X-NUCLEO-MEMS1 function call constructs

Hi,Here is the code from CubeMX generated BSP module for hts221 sensor./** * @brief Read generic device register * * @param hts221_ctx_t* ctx: read / write interface definitions * @param uint8_t reg: register to read * @param uint8_t* d...