SDADC in STM32F373vct6
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-08-22 6:41 PM
hello everybody, I'm a 4th years student and now I'm interesting in stm32. I've started a small project which use SDADC of STM32f373vct6. I've read the referrent manual and configure it as described. But I cant get any result to send through USART1. Please help me to find my mistake . thank you in advanced.
best regards!
#include "main.h"
static __IO uint32_t TimingDelay;
static volatile uint16_t _sdadc_value;
int main()
{
GPIO_config();
USART1_config();
SDADC1_configure();
SDADC_SoftwareStartConv(SDADC1);
if (SysTick_Config(SystemCoreClock / 1000))
while (1);
//USART1_putChar('a');
//while(USART1_getChar() != 'a');
while(1)
{
_sdadc_value = SDADC_GetConversionValue(SDADC1);
USART1_putString("sending");
USART1_putChar(_sdadc_value>>8 | 0x05);
Delay(300);
USART1_putChar(_sdadc_value & 0xff);
USART1_putString("sent");
Delay(200);
}
}
/* Function define */
void GPIO_config(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable clock for GPIOC */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC,ENABLE);
/* Configure GPIOC as Output */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
}
void USART1_config(void)
{
/* Init Struct */
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART1_initStructure;
/* Enable clock for GPIOC */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC,ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);
GPIO_PinAFConfig(GPIOC,GPIO_PinSource4,GPIO_AF_7);
/* Configure PC4(TX) as Output Push Pull */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Configure PC5(RX) as Input floating */
GPIO_PinAFConfig(GPIOC,GPIO_PinSource5,GPIO_AF_7);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Configure USART1 module */
USART_DeInit(USART1);
USART1_initStructure.USART_BaudRate = 9600;
USART1_initStructure.USART_WordLength = USART_WordLength_8b;
USART1_initStructure.USART_Mode = USART_Mode_Tx|USART_Mode_Rx;
USART1_initStructure.USART_Parity = USART_Parity_No;
USART1_initStructure.USART_StopBits = USART_StopBits_1;
USART1_initStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_Init(USART1,&USART1_initStructure);
USART_Cmd(USART1, ENABLE);
/* done! */
}
/* Send data though UART1 */
int USART1_putChar(uint8_t data)
{
USART1->TDR = (data & 0xff);
while(USART_GetFlagStatus(USART1,USART_FLAG_TC) == 0);
return 1;
}
/* send a String though UART1 */
int USART1_putString(uint8_t * data)
{
while(*data != 0)
{
USART1_putChar(*data);
data++;
}
return 1;
}
/* Receive data */
uint8_t USART1_getChar(void)
{
while (USART_GetFlagStatus(USART1,USART_FLAG_RXNE) == RESET);
return ((uint8_t)(USART1->RDR & 0xFF));
}
/* Delay (ms) Fuction */
void Delay(__IO uint32_t nTime)
{
TimingDelay = nTime;
while(TimingDelay != 0);
}
/* Decrement */
void TimingDelay_Decrement(void)
{
if (TimingDelay != 0x00)
TimingDelay --;
}
void SDADC1_configure(void)
{
/* Init Structure */
GPIO_InitTypeDef GPIOE_InitStruct;
SDADC_InitTypeDef SDADC1_InitStruct;
SDADC_AINStructTypeDef SDADC1_AIN_InitStruct;
/* Enable clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE,ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SDADC1,ENABLE);
RCC_SDADCCLKConfig(RCC_SDADCCLK_SYSCLK_Div12);
SDADC_InitModeCmd(SDADC1,ENABLE);
/* PE12 & PE13 are configured in Analog mode */
GPIOE_InitStruct.GPIO_Pin = GPIO_Pin_12|GPIO_Pin_13;
GPIOE_InitStruct.GPIO_Mode = GPIO_Mode_AN;
GPIOE_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOE,&GPIOE_InitStruct);
/* SDADC Init structure definition */
SDADC1_InitStruct.SDADC_Channel = SDADC_Channel_0;
SDADC1_InitStruct.SDADC_ContinuousConvMode = ENABLE;
SDADC1_InitStruct.SDADC_FastConversionMode = ENABLE;
/* Configure Analog Input */
SDADC1_AIN_InitStruct.SDADC_InputMode = SDADC_InputMode_Diff;
SDADC1_AIN_InitStruct.SDADC_Gain = SDADC_Gain_1;
SDADC1_AIN_InitStruct.SDADC_CommonMode = SDADC_CommonMode_VDDA_2;
SDADC1_AIN_InitStruct.SDADC_Offset = 0x000007FF;
SDADC_VREFSelect(SDADC_VREF_VDDA);
SDADC_Init(SDADC1,&SDADC1_InitStruct);
SDADC_AINInit(SDADC1,SDADC_Conf_0,&SDADC1_AIN_InitStruct);
SDADC_ChannelConfig(SDADC1,SDADC_Channel_0,SDADC_Conf_0);
SDADC_CalibrationSequenceConfig(SDADC1,SDADC_CalibrationSequence_1);
SDADC_InitModeCmd(SDADC1,DISABLE);
SDADC_StartCalibration(SDADC1);
SDADC_Cmd(SDADC1,ENABLE);
}
void SPI_configure(void)
{
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA|RCC_AHBPeriph_GPIOB, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1,ENABLE);
GPIO_InitTypeDef GPIO_SPI1_InitStruct;
/**SPI1 GPIO Configuration
PA5 ------> SPI1_SCK
PA6 ------> SPI1_MISO
PB0 ------> SPI1_MOSI
*/
GPIO_SPI1_InitStruct.GPIO_Pin = GPIO_Pin_5|GPIO_Pin_6;
GPIO_SPI1_InitStruct.GPIO_Mode = GPIO_Mode_AF;
GPIO_SPI1_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_SPI1_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_SPI1_InitStruct);
GPIO_SPI1_InitStruct.GPIO_Pin = GPIO_Pin_0;
GPIO_SPI1_InitStruct.GPIO_Mode = GPIO_Mode_AF;
GPIO_SPI1_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_SPI1_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_SPI1_InitStruct);
GPIO_PinAFConfig(GPIOA,GPIO_PinSource5,GPIO_AF_5);
GPIO_PinAFConfig(GPIOA,GPIO_PinSource6,GPIO_AF_5);
GPIO_PinAFConfig(GPIOB,GPIO_PinSource0,GPIO_AF_5);
/*SPI1 configuration*/
SPI_InitTypeDef SPI1_InitStruct;
SPI1_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI1_InitStruct.SPI_CPHA = SPI_CPHA_1Edge;
SPI1_InitStruct.SPI_CPOL = SPI_CPOL_Low;
SPI1_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4; // 72MHz/4 => 18MBits/s
SPI1_InitStruct.SPI_DataSize = SPI_DataSize_8b;
SPI1_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB;
SPI1_InitStruct.SPI_Mode = SPI_Mode_Master;
SPI1_InitStruct.SPI_NSS = SPI_NSS_Soft;
SPI_Init(SPI1,&SPI1_InitStruct);
SPI_Cmd(SPI1,ENABLE);
}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0