STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

why stm32cube programmer cant recognize DFU ?

Hi stm32cube programmer cant recognize DFU.micro stm32f407 board Catalyst F400zdriver installed and DFU device exist in windows 7 device manager.a 1.2k resistor pulled up to pa12 but was useless.run as administrator is tried and was unsuccessful.DfuS...

SChar.8 by Associate II
  • 1548 Views
  • 1 replies
  • 0 kudos

virtual com port driver for ubuntu

I HAVE ONE RFID BOARD WHICH IS HAVING STM32F103C8T6 THIS ONE WILL RUN ON WINDOWS USING VIRTUAL COM PORT DRIVER.BUT I WANT THE SAME BOARD TO USE IN UBUNTU 14.04 BUT I HAVENT FOUND ANY DRIVER FOR UBUNTU TO USE MY BOARD .IS THERE ANY SOLUTION FOR THIS B...

PREDD.2 by Associate
  • 991 Views
  • 0 replies
  • 0 kudos

Float variables print on Debug UART

With the help of STM32 CUBEMX generated basic code for IAR-EW and I have design a small code to print float variables on UART for debug purpose in STM32F413RH. This is working fine in IAR-EW but same things when I used in Atollic TrueStudio it is not...

AP_040 by Senior
  • 1212 Views
  • 1 replies
  • 0 kudos

STM32F429 SDRAM and FMC/LTDC/DMA2D priorities

Posted on October 04, 2015 at 15:16Hello!I'm trying to run STemWin/FreeRTOS/HAL on STM32F429IG revision Y at 168MHz.SDRAM (IS42S16400J-7TLI) connected to FMC controller and runs fine by itself (CAS_LATENCY_3/CLOCK_PERIOD_2/RBURST_ENABLE/RPIPE_DELAY_...

SDIO doesn't work - STM32F429ZIT - FreeRTOS - CubeMX 5.0

Hi,I had a working project on the STM32F4-Discovery board (STM32F407) with FreeRTOS and FATFS on uSD card. I wanted to move to the STM32F429 because the FMC provides a lot of flexibility over the FSMC for my project. For the life of me, I couldn't g...

Zaher by Senior II
  • 1759 Views
  • 4 replies
  • 0 kudos

The original software embedded in

Hi Everyone!I've been working with STM32F769I-Disco & STM32H753I-Eval boards, and I lost the original / demo software / demo firmware / with which both boards comes.Please, Can you help me in the way to find both software packages? In st.com WEB page...

alephian by Associate
  • 995 Views
  • 2 replies
  • 1 kudos

Invalid RTC readings after initialisation.

Hi I am using the RTC on the STM32L433 processor , and works well in periodic and Alarm. I can read in the date and time without any issues within these interupts. But after the RTC is initialised for the first time, reading the date and time regis...

STM32F730R8 status

Hi there,For my upcoming project I am planning to use STM32F730R8. Which is suitable for all the requirement I have. Can you suggest me is it a good dicision. Or this model is on the way for obsolete. Because I need this controller at least 5 years....

Hacha by Associate
  • 932 Views
  • 1 replies
  • 0 kudos

Regarding Controlling of DAC in STM32F303

HelloI'm trying to implement 4-20mA output using DAC CH1. I found out a strange phenomenon during the experiment for the DAC output test.the issue has at both non-triggered mode and software trigger mode of DAC.[phenomenon]I found that the DAC output...