User Activity

Use two NUCLEO-H743ZI boards for SPI communication. Full-duplex DMA mode. When the baud rate is 25M, the master and the slave can receive the data correctly. At 50M and 100M, the slave can receive the data correctly, but the master cannot receive the...
The TCP network of NETX generated by CubeMX does not run successfully.I have studied ST's NETXduo example and tried many possibilities, but it still doesn't work. The development board is NUCLEO-H743ZI.
How to use the hardware CORDIC of STM32G4 to solve the natural logarithm? Are there any examples?
Kudos from