STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to obtain a Burst Write and/or read of external PSRAM

I think the configuration is OK but I don't know how to have a burst Write and/or Read operation.My goal is to have the fastest possible data transfer with a burst lenght of 128 bytes.Having a look at HAL I can't identify the correct function to be u...

MDi L.9 by Associate
  • 1784 Views
  • 2 replies
  • 0 kudos

STM32F103C8 Incorrect HCLK Issue

Posted on February 04, 2016 at 06:05 I am using a minimal develpment board based on STM32F103C8. The board has an external crystal of 8Mhz. I am trying to use PLL as my clock source (with input from HSE 8Mhz) upon boot but facing the foll...

Ethernet

Can't we connect ethernet port(ARJE0034) to controller directly without using ethernet fiji?

saiteja by Associate II
  • 1208 Views
  • 2 replies
  • 0 kudos

Reinitilaization of ADC3 in DMA mode not working

Hey Guys,Iam using a STM32F429IDISCOVERY board with ADC3 in dma mode. Sometimes on special usage circumstances ( a lot of stuff is happening in parallel) there is an overrun error, because the processor is not fast enough to get the packages. Normall...

Switch over RTC from LSE to LSI while running

Hello all!Using STM32L433, RTC is initialized with LSE, works fine.In run, I want to switch to LSI and do certain steps and want to get back to LSE. What is the way to switch over RTC source LSE<->LSI ? I read some thing about backup domain. Please g...

SPate.7 by Associate
  • 2394 Views
  • 3 replies
  • 0 kudos