STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

9 bit UART and DMA

Posted on September 18, 2017 at 07:46Hiya,I'm using the UART in 9 bit mode, with the 9th bit being used as an address indication.I have a version of this working well with 16 bit DMA transfers. Ideally though I want to use 8 bit DMA (byte wide) as a...

l m by Associate II
  • 5354 Views
  • 7 replies
  • 0 kudos

Problems with CAN on STM32F072RB

Hi, I'm trying to implement CAN on the STM32F072RB and I think I have added all the neccesary files. In stm32f0xx_hal_conf.h I have defined HAL_CAN_MODULE_ENABLED, but in stm32f0xx_hal_can.c it is not recognized. The question is that when compiling e...

pfc1 by Associate
  • 604 Views
  • 0 replies
  • 0 kudos

How I use CubeMX with bluenrg-2?

Posted on December 18, 2017 at 22:07I would like to create a program using CubeMX support program(like the one used for the STM32 family).Followed by loading into Keil_v5 and then flash the code into the BlueNRG-2 chip.Please advise how it can be do...

STM32H7 External 8mHz osc & PLL to 400mHz settings

Posted on July 07, 2018 at 10:37 Hi everyone, I've been using the STM32H7 Nucleo board (STM32H743ZI) for a project I'm working on. I'm using plain CMSIS (no HAL solutions please ) and I'm having a bit of trouble setting the clock settings to u...

Wakeup from STOP2 sleep using RTC Alarm

I'm trying to wake my STM32L471 up from STOP2 sleep mode using the RTC Alarm. I successfully get it to sleep, and then I'm using the code from the STMCube Example projects (\STM32Cube_FW_L0_V1.11.0) to try to wake it, but not succeeding. Is anyone ab...

Audio output via onboard DAC's

Hi guys, I've never done this before but has anyone used the onboard DACS to produce sound? Playing a .wav file.I know the dacs are only 12bit and it should play 8bit wave samples fine but what about 16bit samples?I'll be receiving my MCU's next week...

PAdam.6 by Associate II
  • 10631 Views
  • 8 replies
  • 0 kudos