STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F103: HSE Crystal Capacitors

Hello Which are the correct Capacitors to use for HSE on STM32F103 with the following Crystal?Frequency: 8 MHzLoad capacitance CL: 20 pF Thank you in advance for a quick hint.RegardsMichael 

Resolved! Crystals and load capacitors for stm32l432

Posted on July 10, 2018 at 14:37I've been designing sub-gram boards for data logging on songbirds using the stm32l432.  Although mostly I use ultra-low power external RTCs, I recently built a test board using a 4pf 32768 crystal.  The question was t...

Resolved! STM32 HSE Crystal

Hello, I'm using an STM32H750VB and am trying to use the HSE crystal to communicate over USB to my computer, but it isn't able to connect to my computer. I suspect that the issue lies with the crystal since I tried to probe it with an oscilloscope an...

Avid_0-1740015744386.png Avid_1-1740015879677.png
Avid by Associate III
  • 2248 Views
  • 3 replies
  • 0 kudos

Resolved! USB product string no visible on host

Hi,I have developed custom board with STM32C071CBT6. I configured USB port with USBX in CDC mode. I configured USB device descriptor values as below: When I connect host Windows 11 PC to my custom board, device manager on PC shows - USB Serial Device...

PPate1_0-1744892248308.png
PPate.1 by Associate III
  • 1401 Views
  • 2 replies
  • 5 kudos

Resolved! STM32L431 CANBUS Bootloader problems

Hi all,I'm struggling to get the ST bootloader on a STM32L431KUB to communicate with a STLINK-V3SET via CANBUS using the STM32CubeProgrammer, the reported error is ST-LINK error (BRG_CAN_ERR) Establishing connection with the device failed.I have made...

monsi by Associate
  • 1045 Views
  • 1 replies
  • 0 kudos

Radiation immunity documents required

Hello Team,We are using STM32F765IIT7 MCU.We would like to get the radiated immunity document if tested (to get a understanding how good this controller is with single event effect)Kindly share any supporting documents.Best Regards,Yuvakumar

yuva by Associate
  • 808 Views
  • 1 replies
  • 1 kudos

SPI transmition stop after first 4bits

Hello I'm using trying to access to an external flash through the SPII try to send 5 bytes, my SPI transmit function work well if I put some delay (1us) between each byte, if I don't put this delay transmission start and stop just after 4bits.green -...

andre239955_stm1_stmicro_0-1744810925721.png andre239955_stm1_stmicro_1-1744811271887.png andre239955_stm1_stmicro_2-1744811441425.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.