STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem while receiving data from MEMS microphone.

I am using the STM32F407 discovery board and Wolfson pi audio interface. I have a problem in analysing sample values received from MEMS microphone.I wanted to plot the data sensed by the MEMS microphone, which is just sensing the surrounding environm...

rrach by Associate II
  • 1807 Views
  • 3 replies
  • 0 kudos

I2C by IT [solved]

Hi,I use I2C like this uint16_t I2cAddrTemp = 0x90; uint8_t I2cWritedata = 0x00; uint8_t I2cReaddata = 0xFF;   uint8_t read_i2c_temp(void) { hi2c1_status = HAL_I2C_Master_Transmit(&hi2c1, I2cAddrTemp, &I2cWritedata, 1, 1000); //PRINTF("I2c = %02X",...

MMath.10 by Associate II
  • 1220 Views
  • 0 replies
  • 0 kudos

Plug-in "com.st.microxplorer.rcp" was unable to instantiate class "com.st.microxplorer.eclipse.rcp.MicroXplorerView".

Hello, I've installed Eclipse IDE for C/C++ Dev (V. Oxygen.3a release 4.7.3a) in Windows 10.I've installed stm32 cube mx plugin (en.stsw-stm32095.zip) following procedure on UM1718 user manual ("Installing STM32CubeMX as an Eclipse IDE plug-in" parag...

LucaCMA by Associate II
  • 659 Views
  • 0 replies
  • 0 kudos

I2C2+DMA1 and UART4+DMA1

Hi all,I'm having some trouble getting DMA to service sequential uses of I2C+DMA transactions.​​​I can have the I2C+DMA initialize our demodulator, which involves some 12,000 reads and writes. (So, I2C+DMA works *very, very well* when it works.) I ca...

EJohn.17 by Associate II
  • 1888 Views
  • 3 replies
  • 0 kudos

STM32F407 SDIO/SDCard

Posted on March 29, 2018 at 04:32I am trying to get the STM407VET to communicate to an SD Card using the SDIO interface and drivers. Code base was generated from CubeMX and Eclipse is the IDE. Debugging with Open OCD. Hardware is custom. I have trac...

Resolved! FMC memory map confusion

Hello,I have a little confusion regarding FMC memory map. I hope someone can help me with it.Accoring to reference (stm32h743) FMC external memories are mapped as following:0x6C000000 -0x6FFFFFFF FMC NOR/PSRAM/SRAM 4 Bank1 (or remap of FMC SDRAM Ban...

ranran by Senior II
  • 4881 Views
  • 3 replies
  • 0 kudos

Hard fault caused by strncpy,

Hi,I am running into a strange problem, I am using strncpy function to copy one array into another. If i include this in my code i get a Hard fault DEBUG_VT . I have read quite few article on hard faults and how to track them down but this one that i...

conrad c by Associate II
  • 2632 Views
  • 3 replies
  • 0 kudos

Resolved! Help getting started with NUCLEO-F722ZE

So I've just bought a F722ZE based board which is ideal for the projects I'll be working on, however I was hoping I could get this to work with the arduino IDE and save myself the trouble of learning the new platform, but this doesn't seem to be poss...

JWood by Associate II
  • 2260 Views
  • 3 replies
  • 0 kudos