STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART Interrupt STM32F103ZET6

Hello all.I am new working with the SMT32 microcontrollers and I need your help.The project deals with 3 communication channels USART to 19200bds (usart1, usart2 and usart3)The microcontroller used is the STM32F103ZET6 and would be connected to 3 dif...

DGonc by Associate II
  • 2121 Views
  • 3 replies
  • 0 kudos

ST-Link debugging problem / ST-Link Utility problem

Posted on February 26, 2018 at 18:10 Hi, I was doing my thing, writting and debugging code with System Workbench and after a while ST-Link refused to work anymore, out of the blue. I had not changed SWD pins nor related settings. It just stopped ...

Resolved! stm32f103 14mhz adc clock and prescalers only allow 12mhz?

hi i'm reviewing rm0008 ref manual for stm32f103 the adc.accordingly, adc clock max is 14mhz and it takes 14 adc clock cycles for 1 conversion - hence 1msps per ADC.however, from the RCC section the available prescalers are 2, 4, 6, 8and if we take 7...

andrewg by Associate III
  • 2349 Views
  • 2 replies
  • 0 kudos

HardFault_Handler

Hi, I have a problem with HardFault_Handler.Sometimes, when I'm writing into the flash it happens.After many days on searching still I don't understand why it happens and what it means.Has someone got a suggestiom for me?

Expanding on ISRs generated by CubeMX

Dear AllCubeMX (Clive, I know you do not encourage relying on it, but please bear with me for a while) adds many c and h files to a project. Is the programmer allowed to modify any of such c files other than the main.c? For example, I see a void SyST...

Amir1 by Associate II
  • 827 Views
  • 0 replies
  • 0 kudos

ROS spinOnce jamming the process of MCU

We are using ROS Serial to let Raspberry Pi and STM32F103C8T6 communicate with each other. And there is another UART channel for IMU to use. We observe that the spinOnce function of ROS jammed the process of MCU. Therefore, other work cannot operate ...