STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L072 Discovery Board cannot receive the UART data

Hi,I'm using STM32L072 Discovery Board and generated UART code using CubeMx, I'm able to transmit the data via UART but not able to receive the data. Please help me in this regard.int main(void) { /* USER CODE BEGIN 1 */   /* USER CODE END 1 */  ...

Backup data from the RTC when the main power is cut off

Hello everyone, I'm using RTC on board NUCLEO-L053R8, so I have some problems. How do I connect a battery in this board? I know that if I want save my battery lifetime I have to put my microcontroler in a mode as StopMode, but how can I do that when ...

VOliv.5 by Associate II
  • 1018 Views
  • 1 replies
  • 0 kudos

STM32H743 HRtimer PWM

hi i'm using HRTIM for PWM output.i could complete pwm output. but i want to stop it at pulse count that I want.is there any good way to stop output at i set pulse counts??​

klee.15 by Associate
  • 1332 Views
  • 2 replies
  • 0 kudos

H750VBT6 BKPSRAM can't keep DATA

 /* Enable write access to Backup domain */ PWR->CR1 |= PWR_CR1_DBP; while((PWR->CR1 & PWR_CR1_DBP) == RESET) { } /*Enable BKPRAM clock*/ __HAL_RCC_BKPRAM_CLK_ENABLE();   *(__IO uint32_t*)(0x38800000+36) = 12345678;run to here, DATA 12345678 is writt...

ZYubi by Associate III
  • 1361 Views
  • 2 replies
  • 0 kudos

DMA Overhead (ADC to RAM)

STM32F446 in my case...When the ADC finishes a conversion and the DMA controller deposits the converter data into memory, what is the overhead ? i.e. How long does it take ? Is this shown in the documentation anywhere ?I would assume that as soon as ...