User Activity

Hello We are unable to write into USBH registers in stm32mp157. Actually, we enabled USBHEN and USBHLPEN bits in AHB6ENSETR and AHB6LPENSETR registers. Then we are unable to access USB memory. We tried other peripherals same way means en...
Actually, we are trying to reset the MAC registers by using DMA mode register (bit 0) in Ethernet section.As per reference manual, we are set the bit(swr bit) to 1 in ETH_DMAMR_REG register. but it is not reset automatically. In software we done // E...
Hi , We are using the STM32MP157-dk1 board. We are able to boot the both cores (cortex A7) bare metal code from the SRAM but where as loading to the DDR that time only core 0 is booting properly and core 1 not booting. Is their any way to enable the...
we are trying to program a hex file by using st link v2 programmer in cube programmer getting follow error.no stm32 target found.also I updated the firmware.the target board is working with another st link.from not working st link we are getting TCK ...
We are using St distribution source code and we compile the source code in buildroot tool. But we unable to get User login page. How can i get the User login page.Would you help in this regards.Thanks in Advance.
Kudos from