2018-09-22 6:12 PM
Hello,
I have the L432KC Nucleo. I'm trying to measure low speeds with a 1 PPR (pulse per revolution) sensor. For low PPRs. using the Period Measurement Method is suggested. If I get the period of the signal, then I can apply the formula:
RPM = 60/(Pulse Period)
It's my first time using input capture mode. This is what I have:
In CubeMx I've set Timer 2, channel 3. My APB2 frequency is 1 MHz. The TIM2 prescaler is 1000 and the counter period is 10000. Everytime a pulse is given, a falling edge occurs. Is everything good so far?
Now, in the code I have:
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
{
/* Prevent unused argument(s) compilation warning */
UNUSED(htim);
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_TIM_IC_CaptureCallback could be implemented in the user file
*/
if(htim->Instance == TIM2){
inputCaptureVal = __HAL_TIM_GetCounter(htim);
__HAL_TIM_SetCounter(htim,0);
}
}In the while loop I have another variable: counterVal= __HAL_TIM_GetCounter(htim2);
I'm kind of lost. Is this the right way to get the period? I would appreciate any guidance.
2018-09-22 7:42 PM
Wouldn't the capture event load CCR3 with the value of CNT at the event?
I would tend to use PWM Input mode where CH1/CH2 would provide a Period and Duty value, and reset the count.
The other method is to have the counter in a maximal mode ie ARR=0xFFFFFFFF for a 32-bit TIM, and then subtract the last value of CCR3 from the current to get a delta ticks measurement. This would have less issues with latency.
In maximal mode you can use uint32_t a, b, delta; where delta = b - a; for all values.
2018-09-23 2:52 PM
Is this routine okay?
// PWM Input Mode
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) {
if(htim->instance == TIM2) {
if(htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {
//if CH1 is rising
IC1Value = HAL_TIM_ReadCaptureValue(htim, TIM_CHANNEL_1); //Read CH1 value
TIM->CNT=0 // Reset count
Period = IC1Value;
}
}
}
2018-09-24 9:28 AM
Hi @XP.1acheco ,
I really advise you to refer to "TIM_InputCapture" and "TIM_PWMInput" examples provided under STM32L4 Cube package:
STM32Cube_FW_L4_V1.13.0\Projects\NUCLEO-L432KC\Examples\TIM
The examples are well explained and will help you to understand how to use the timer peripheral under the Input capture and PWM input mode.
Khouloud.
2018-09-24 5:27 PM
Hi @Khouloud GARSI Thank you. I was looking into the PWM Input Example:
Does the count reset automatically? As I'm interested in measuring the pulse period to find the speed, the only essential line is
uwIC2Value = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_2); Right?
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
{
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_2)
{
/* Get the Input Capture value */
uwIC2Value = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_2);
if (uwIC2Value != 0)
{
/* Duty cycle computation */
uwDutyCycle = ((HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1)) * 100) / uwIC2Value;
/* uwFrequency computation
TIM2 counter clock = (RCC_Clocks.HCLK_Frequency) */
uwFrequency = (HAL_RCC_GetHCLKFreq()) / uwIC2Value;
}
else
{
uwDutyCycle = 0;
uwFrequency = 0;
}
}
}
2018-09-26 8:26 AM
Hi @XP.1acheco ,
The answer is YES for the two questions.
Khouloud.