Skip to main content
Johanan1
Associate III
September 27, 2018
Question

can't use TIM21 as pulse counter STM32L051

  • September 27, 2018
  • 5 replies
  • 1161 views

I try to count pulses from PA1 as TIM21_ETR, seems like all setting is OK, but no counting what soever. What am I missing?

Thanks

/* TIM21 init function */
void MX_TIM21_Init(void)
{
 TIM_ClockConfigTypeDef sClockSourceConfig;
 TIM_MasterConfigTypeDef sMasterConfig;
 
 htim21.Instance = TIM21;
 htim21.Init.Prescaler = 0;
 htim21.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim21.Init.Period = 0;
 htim21.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 if (HAL_TIM_Base_Init(&htim21) != HAL_OK)
 {
 Error_Handler();
 }
 
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_ETRMODE2;
 sClockSourceConfig.ClockPolarity = TIM_CLOCKPOLARITY_NONINVERTED;
 sClockSourceConfig.ClockPrescaler = TIM_CLOCKPRESCALER_DIV1;
 sClockSourceConfig.ClockFilter = 0;
 if (HAL_TIM_ConfigClockSource(&htim21, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim21, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 HAL_TIM_Base_MspInit(&htim21);
}
 
 
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle)
{
 
 GPIO_InitTypeDef GPIO_InitStruct;
 if(tim_baseHandle->Instance==TIM21)
 {
 /* USER CODE BEGIN TIM21_MspInit 0 */
 
 /* USER CODE END TIM21_MspInit 0 */
 /* TIM21 clock enable */
 __HAL_RCC_TIM21_CLK_ENABLE();
 
 /**TIM21 GPIO Configuration 
 PA1 ------> TIM21_ETR 
 */
 GPIO_InitStruct.Pin = GPIO_PIN_1;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF5_TIM21;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /* USER CODE BEGIN TIM21_MspInit 1 */
 
 /* USER CODE END TIM21_MspInit 1 */
 }
}

    This topic has been closed for replies.

    5 replies

    waclawek.jan
    Super User
    September 27, 2018

    Read out and check/post content of relevant GPIO and TIM registers.

    JW

    Johanan1
    Johanan1Author
    Associate III
    September 27, 2018

    Thanks, that is strange ( I think).

    All TIM21 registers are 0x0000 except

    SMCR = 0x00004000 and

    SR = 0x00000001

    Johanan1
    Johanan1Author
    Associate III
    September 27, 2018

    GPIOA:

    0690X000006C5k1QAC.png

    Johanan1
    Johanan1Author
    Associate III
    September 27, 2018

    found it, need ARR = 0xFFFF and timer need to be anabled , CR1 = 0x01

    waclawek.jan
    Super User
    September 27, 2018

    If resolved, mark as so (Best). Thanks.

    JW