STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Some hints on using the SWD interface to program devices

I am soon going crazy! I have used 4 different types of USB -> SWD (Cortex M-10 adapter) programmers like STLINK/V2, Segger J-Link etc. I have made PC boards with several different STM32 MCU types, and what happens is that on some boards the Flash pr...

rolfmyhre by Associate II
  • 1398 Views
  • 2 replies
  • 0 kudos

FAILED to reset/halt the target MCU

when i connect my nucloe f411re with usb, there is a 32kb mass storage. Also st-link utility program doesn't erase chip it error and says "cannot connect the target" but it perform firmware uptade successfuly.how can i reset the board? some people re...

Oladi by Associate II
  • 2485 Views
  • 5 replies
  • 0 kudos

Should SSM be 0 or 1 when using SSOE=1?

According to reference manual section 49.4.7 (Slave select (SS) pin management), “Hardware SS management (SSM = 0): in this case, there are two possible configurations … SS output enable (SSOE = 1)�?.​However, according to reference manual section 49...

CHead by Associate III
  • 1422 Views
  • 1 replies
  • 0 kudos

How can I use my MPU5060 on STM32L432?

I found only a way to read MPU5060's values with STM32F :(I tried it on my STM32L but it seems that the suggested libraries are not compatible with STM32L.Can you help me please ?:)

abj by Associate
  • 673 Views
  • 0 replies
  • 0 kudos

Can running code find out the part number it's running on?

I'm writing code for STM32F042. If I'm running on the TSSOP20 package, I need to remap PA11 and PA12 to PA9 and PA10. For all other packages, I need to leave them alone.I can have a compile-time switch and generate different binaries for different pa...

AKrup by Associate II
  • 2258 Views
  • 4 replies
  • 0 kudos

Example of CAN RTR response message setup

I have the CAN functioning properly on the STM32F413 using Interrupts for Tx and Rx. I now want to add a response to an RTR message using the STM hardware only. I read the Ref Manual CAN chapter and the Datasheet. I understand how CAN functions and h...

KHule by Associate
  • 940 Views
  • 0 replies
  • 0 kudos

SMBUS with MLX90615 I am not able to get desired waveforms

I cant see a continuous clock. I want to put it in master mode and it seems to send only one byte and stops.Heres a snipetArray[0] = 0x27;   HAL_SMBUS_Master_Transmit_IT(&hsmbus3,0xB6, Array, 5, SMBUS_OTHER_FRAME_NO_PEC); while(HAL_SMBUS_GetState(&...