User Activity

I would like to use the Stop3 low-power mode on an STM32U545RE (NUCLEO-U545RE-Q board) and to wake-up the device by the RTC. I have a working example for Stop2 mode for which I largely used the inspiration from the stm32u5 workshop. But when I replac...
Hi,in our STM32MP project, we have some unused securable peripherals. We generate our devicetree bindings with CubeMX where we have not selected anything for these peripherals. Accordingly, they do not show up in the `st,decprot` attribute in the `&e...
In Keil.STM32L4xx_DFP.2.5.0.pack, which can be downloaded at https://www.keil.com/dd2/pack, the memory information for stm32l452 says that the ram size is 0x00020000 = 128kB, but it actually is 0x00028000 = 160kB (SRAM1 + SRAM2).Using this file for m...
We would like to share data between the A7-core and the M4-core on an STM32MP1 device. Those cores both have access to the SRAM1,2,3,4 . The M4-core is connected directly via the AHB interconnect, the A7-core is connected via the AXI-based NIC-400 in...
I am using the HAL library to use my MCUs peripherals and I would like to use the IDLE line detection of the UART controllers. To me, it seems that the HAL library does not offer any callback for IDLE line detection so I think it is not possible to u...
Kudos from
Kudos given to