cancel
Showing results for 
Search instead for 
Did you mean: 

minimum latch time for BOOT0 pin

YCohe
Associate II

Hi,

What is the minimum latch time for BOOT0 pin (after reset) in order to get the MCU to internal ST bootloader mode? Is there timing diagram somewhere?

FYI, I am using STM32L475 MCU.

Thank you,

Yuval

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Imen.D
ST Employee

Hello,

On STM32L475, the Boot0 pin is latched on the rising edge of the NRST pin.

We do not specify an hold time required on this Boot0 pin versus the NRST pin.

Even if the Boot0 pin switches from 1 to 0 immediately after reset release, the MCU will enter bootloader mode.

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
in mozbek we trust
Associate II

It is 4 SYSCLK after reset

Any source? Link?

JW

Thank you for your answer.

Let me just make sure I understand, once NRST goes high, Boot0 latch time should only be > 0. Is my understanding correct?