STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! NUCLEO-F722ZE I2C2 in slave mode doesn't work nothing.

Hi,I am using NUCLEO -F722ZE board for testing the STM32F7 and their peripheral features. Other peripherals I tested works fine, but I have encountered a problem with I2C2 in slave mode, that doesn't send ACK when the master calls it (status flags ke...

0690X0000088scvQAA.bmp
RCata by Associate III
  • 849 Views
  • 1 replies
  • 0 kudos

GPIO Speed

Hello everybody,I have to generate a pulse with very narrow and different widths. The setting and procedure is as follows: Clock Freq = 16 Mhz, Prescaler = 1. off time should be 15 μs,  thuss = 15 μs * 16MHz / 2 = 120  Counts and with this logic for ...

Samuel1 by Associate III
  • 1851 Views
  • 3 replies
  • 0 kudos

Why placing breakpoints after enabling and starting USART DMA transfer in STM32F429I Discovery board corrupts my program execution?

Hi EveryoneI am working on a FreeRTOS based application in which I have to enable USART DMA channel to transmit 16 bytes of buffer from memory to USART Data Register in a task. It happens every time my task is invoked. Everything seems to work fine u...

MSaif by Associate II
  • 1577 Views
  • 2 replies
  • 0 kudos

multi master spi

Hey everyone,I've been struggling with the multi-master spi. I can send and receive seperately but when I try to integrate it into one program it bogs out. My understanding is that I can set the SPI line as a slave and then whenever I want it to act ...

con3 by Senior
  • 3261 Views
  • 7 replies
  • 0 kudos

No Output Voltage from TI DAC chip,with stm32F7

Hi,there.I am using DAC60508 with my STM32F7,60508 is 12 bits precision,and with 24 bits command-length,SPI interface. After initialize the SPI,I send 3 bytes separately,and I use a oscilloscope to check the wave of SCL�?SDI�?CS,its seems right,but i...

0690X0000088nakQAA.png
YShiw by Associate
  • 1296 Views
  • 1 replies
  • 0 kudos

Looking at getting 1st STM32...

My main goto board ATM has been an Arduino Due as it has heaps of pins, 3.3v, 32 bit , 96K or SRAM, 512K of flash and easy to program straight from Visual Studio.One thing I hate about it is all they all seem to ship with female header pins and the l...

DWhit.1 by Associate II
  • 1456 Views
  • 2 replies
  • 0 kudos

stm32f030f4p6 HAL_UART_Receive dont work

I'm using stm32f030f4p6. The system clock frequency is 8mhz. uart1 setting 9600, n, 8.1. I am using the following program code. wotchdog stm32f030f4p6 uart is running smoothly when I send 18 123456123456123456 characters from my computer serial port ...

bg??k by Associate
  • 1109 Views
  • 1 replies
  • 0 kudos