hande
Associate II
since
2018-11-04
2023-06-14
User statistics
7
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About hande
Options
Report User
User Activity
Posts
Replies
has anyone ever made a STM32 project with an infrared sensor by using PWM on the transmitter pin. the result of my sensor isn't running
2018-11-07
how to convert uint8_t to string
2018-11-07
how to convert uint8_t to string and show in SSD1306_Putsi try like this.uint8_t check;SSD1306_Puts("choose dreep"+String(uint8_t), &Font_7x10, 1);
is there a way to make a button click and double click?
2018-11-04
I tried to make it use timers and counters but it didn't work well. please help
Re: how to convert uint8_t to string
2018-11-07
Okay thank you very much AvaTar.
Re: how to convert uint8_t to string
2018-11-07
is it written like this. please help SSD1306_Puts((uint8_t*)check, &Font_11x18, 0);
Re: is there a way to make a button click and double click?
2018-11-04
thank you, maybe there are video suggestions or tutorial blogs that are like this case
Re: is there a way to make a button click and double click?
2018-11-04
sorry, I still don't understand. i use stm32cubemx, true studio and hal library.