STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I need to have a function that is being called everytime my DMA transfered all the data to my LEDs. How can I do that? Thanks for your answers!

Hi everyone! I am using STM32F446RE for a project of Tetris with a LEDs matrix (WS2812B). To communicate with my LEDs, I call HAL_TIM_PWM_Start_DMA(&htim2, TIM_CHANNEL_4, (uint32_t*)pixelsBuff, (uint16_t)pixelsBuffSize) every 500 ms. And this works w...

ARey.17 by Associate
  • 540 Views
  • 0 replies
  • 0 kudos

STM32L0 strange current draw from stop mode

I have encountered a strange power draw behavior of an STM32L0 device in a battery powered circuit. Using a Nordic power profiler kit, the device draws the nominal 5 uA current after entering Stop mode then seems to "wake-up" and draw 78 mA. The curr...

KBrow by Associate
  • 1320 Views
  • 0 replies
  • 0 kudos

SDIO Hardware Flow Control

Posted on December 17, 2013 at 05:03Greetings all, I've been playing around with SDIO on an STM32F4 -Discovery card with the Embest Baseboard on it. My goal is to get it to work in polling mode, flow control mode, interrupt mode, and dma mode. This ...

orders-st by Associate II
  • 3286 Views
  • 2 replies
  • 0 kudos

STM32L4xx Internal RTC Timestamp

Hey, I try to get timestamp from tamper event when mcu supplied with VBAT, but value oftimestamp still 0, can anyone help me ?

dobs by Associate II
  • 1375 Views
  • 2 replies
  • 0 kudos

DFU and DFUSE for STM32L476 Discovery Problem

Posted on October 22, 2016 at 16:36Hello,I am having an issue with DFU downloading to a STM32L476 Discovery board.- Compiled a simple LED switching application in IAR converted to DFU by the file manager (tried both bin and hex)- Tested via ST-LINK ...

imalamoud by Associate II
  • 1241 Views
  • 2 replies
  • 0 kudos