STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Delay Chip select line STM32U5 OSPI

I am using the NUCLEO-U575ZI-Q.I am using the OSPI peripheral in QSPI mode.The device I am communicating with needs a longer delay after the CS line is asserted low.I have tried setting the "ChipSelectHighTime" to 8, but I think this only affects the...

LCorb2_0-1744062313679.png
LCorb.2 by Associate II
  • 1807 Views
  • 4 replies
  • 1 kudos

STM32H753VIH6 RMII Signal Validation

Hi Team,We are using the STM32H753VIH6 in our design.We are connecting the Realtek RTL8364 through RMII interface.I have powered the STM with 3V3.Attached the waveforms for undershoot and overshoot accepted levels.This has been probed with 2GHz Oscil...

stm32g0 timer input capture division does not work

Hello!Using TIM1 for pwm input capture.Works OK for trigger prescaler 1 (default).Want to use prescaler 4, but it doesn't work. Capture value the same as prescaler 1. Timer config:void FC_SERVO_1_TIM1_Init(void) { // USER CODE END TIM1_MspInit GPI...

Bigdan by Associate III
  • 2193 Views
  • 7 replies
  • 3 kudos

Stm32f429i-disc sdram fb with ltdc

Hy,  i am new here and need help. Is there an exemple of a cube ide project with all the important files like .ioc ect.?I have problems with the onboard display.I use the sdram bank2 as framebuffer (startaddress 0xd0000000). I can see (mem window) th...

Interfacing the LTC1403 SPI ADC

Hi there,I'm currently trying to get SPI Communication with the LTC1403 up and running, however I'm struggling with the timing of the Conv Signal.It seems like I need the rising edge of SCK at the same time as the Conv Signal is high. How can I achie...

always_energized_0-1745156290531.png

Resolved! Synchronous start of three timers

Hello everyone. Question about synchronous launch of three timers.Given:- CPU F0 or F4 or G4 (of course F103 is possible - I just don't like it, personal dislike);- three timers, each with its own operating frequency, Timers work via DMA, each with i...

Aflik by Associate II
  • 1115 Views
  • 2 replies
  • 0 kudos