STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! reset problem

hi, im using stm32g474vet6 mcu for power converter. when the supply is turned on initially first time, controller is behaving like hang or stuck somewhere. if i do a pushbutton reset, the mcu starts working fine. after that no issue. whenever im turn...

Resolved! STM32F030R8 PSPICE model

Hi, As I am doing a Pspice simulation, for which I am using STM32F030R8, I need the Pspice model of STM32F030R8. To use the GPIO Functionality to connect the MCU to the simulation circuit in LTspice or OrCAD Pspice.

nandhini by Associate
  • 1120 Views
  • 1 replies
  • 1 kudos

Resolved! 800KHz Frequency generation using STM32G070RBT6

I am trying to get 800KHz frequency with Timer 3 and timer clock is 64MHz and i am using below setting to initalize the timer, but its frequency is 666.66KHz. Pls provide a solution of this problem ASAP......   static void MX_TIM3_Init(void) { /...

Preetpal by Associate II
  • 1594 Views
  • 2 replies
  • 2 kudos

devnonce is too small

hi guys,I am experiencing an issue related to the "devnonce is too small" error. When I attempt to switch end nodes in the TTN network, I change the end node network keys (such as Join EUI, Dev EUI, and App Key) through USART. I stop the LoRa MAC, de...

kRaje.1 by Associate II
  • 888 Views
  • 1 replies
  • 0 kudos

STM32G4 UCPD:Debug issue

Hello, I have encountered a similar problem to the one in this link .I am also trying to use the UCPD Monitor to send message. For example, I request a new voltage from the source using the "Request Power Profile" message from the "Message Selector" ...

Susu_0-1741242599589.png Susu_1-1741242623726.png
Susu by Associate II
  • 2658 Views
  • 5 replies
  • 0 kudos