User Activity

I need to measure 0 to 80V DC voltage with STM32F373CCT6 and I have some questions to get the best performance of the SDADC.*Is this CPU and 16-bit SDADC good for this purpose?*Is it better to use the internal 1V8 Vref or an external 1V8 or 3V3 Vref?...
Hi, I have a STM32G474 connected to a Quectel LTE module via a uart4 and a GPIO pin.Under normal conditions is it possible for the CPU to boot from flash and when the quectel changes the level of the gpio pin of the STm32, the CPU jump to boot from u...
Hi all.I would like to use the VN5T016AH-E high-side driver and I have some questions.*Are there 8V in the CS pin under fault conditions?*Can it measure max 4.2A with a K about 4240? Why do you specify 4V in the datasheet without knowing the value of...
Hi at all.Can VNLD5160 work with a normal STM32 CPU with 3.3V logical levels?I don't find this information in datasheet...Thanks...
Hi all.Why when I configure an ADC input in PA2 port, I have a conflict with another pin PA3 port that is configured as GPIO?Many thanks. 
Kudos given to