STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! QUADSPI MDMA problem

Hello,I am working on indirect read of quadspi using MDMA. Regular pooling worked fine without any problem. I have 4 line dual buffer QSPI circuit. I used HAL function HAL_QSPI_Receive_DMA(&hqspi, data);No data read from qspi. Moreover I have found i...

BBlas by Associate II
  • 3011 Views
  • 4 replies
  • 0 kudos

what does the datasheet mean ?

what does the datasheet mean ? This is the STM32F103C8's datasheet.In Medium-density devices has 1xPWM timer and 3x16bit timers.​​i know that 16bit timer can be PWM function.What is the difference between 16bit timer and PWM timer?​​STM32F103C8 timer...

0690X000008ABP2QAO.png 0690X000008ABPRQA4.png
cTomm by Associate II
  • 1125 Views
  • 2 replies
  • 0 kudos

How to change DMA from 16bit to 8 bit transfers

I have inherited a wadge of working SPI DMA code for a product. I want to send bytes rather than 16 bit words. In order to change the length of the SPI packets from 16 clock cycles to 8, I changed the DMA_CCR1_MSIZE & PSIZE fields in DMA1_Channel3->...

Resolved! Problem with HAL_I2S_DMA_Receive()

I am using STM32f407VG Discovery for audio application. I am having a problem while using the I2S2 in Slave Receive mode using the HAL_I2S_DMA_Receive() for receiving 16-bit data on a 32-bit frame. I am able to get the Audio data correctly at times a...

HKaur by Associate II
  • 1493 Views
  • 2 replies
  • 0 kudos

STM32G070. In the code generated by the CubeMX, there is the colock source is selected for the TIM1/15, TIM1CLockSelection/TIM15CLockSelection. But in datasheet, the clock source is only TIMPCLK and no other source. I think this is the tool bug.

void SystemClock_Config(void){ RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_PeriphCLKInitTypeDef PeriphClkInit = {0}; /** Configure the main internal regulator output voltage  */ HAL_PWREx_ControlVoltage...

Mmei by Associate
  • 700 Views
  • 0 replies
  • 0 kudos

Programming alternatives of the STM32H750VB

Hello,​I would like to ask a question further to my recent one about the Value Line STM32H750 3 weeks ago or so.The chip has 128KB Flash and 1MB RAM.Assume my program is bigger than 128k and I decide to use NOR Flash as a storage and to run from the ...

Yevpator by Associate III
  • 1494 Views
  • 1 replies
  • 0 kudos

Just how powerful are STM32s?

I'm sure this is a pretty loaded question, especially considering that there are a range of them out there now, plus I'm sure it also varies based on application(s), ​im just curious because I am coming from an Arduino world (and going to school to g...