User Activity

We have a Zigbee network, working as a coordinator, and we want to know which devices are connected. In order to know which devices are connected, we use this code: while (ZbNwkGetIndex(zigbee_app_info.zb, ZB_NWK_NIB_ID_NeighborTable, &neighbor, size...
Using the Zigbee stack as a coordinator, is there a callback available to notify when a new device is associated in the network?We observe the following in the M0 log:[M0] [00000015.076][PLATFORM] nwk_handle_assoc : Association accepted, sending resp...
Using TrueStudio we have a post build step which modifies the generated binary file, but using STM32CubeIDE doesn't work because the post build step is executed before the binary file is generated. How I can perform a step after generate the binary f...
Posted on January 03, 2018 at 10:44Hi again,I'm using an RTC as I explained in https://community.st.com/0D50X00009XkWttSAF.Our device have a battery in VBAT, so the RTC still works when the device it's power off. But after a power on the RTC can los...
Posted on January 03, 2018 at 10:22Hi,I'm using a STM32L496VG, with an external LSE of 32768 Hz. I configure the RTC this way:/* Enable Power Control clock */__HAL_RCC_PWR_CLK_ENABLE();/* Enable writing RTC back-up registers */HAL_PWR_EnableBkUpAcce...
Kudos from
Kudos given to