STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [SOLVED] Getting Hard and Usage Faults when setting the HCLK of STM32F411RE to anything above 60MHz

Hi,I'm working on porting a project from the Nucleo-F411 to a custom PCB. Everything works fine when setting the HCLK to 60MHz and below (running from the internal HSI RC clock and PLL), but i'm getting Hard and Usage Faults when setting the HCLK to ...

Resolved! Uart parity issue.

Hi, I am running a STML433 with external xtal. I have a serial port that works fine when I set the parity to NONE (I set the port to 9600 baud No parity 8bits 1stop bit). And works well , as expected. I have to set it to parity even (set to 9600 bau...

ADC Fast \ Slow Channels

Hi,i want to use the ADC to measure 7 Hall sensors,i need the conversion time for all seven ADC channels needs to be the same,i use both slow and fast channels, i have the following questions:1. How to make the conversion time for the slow and fast c...

PBerg by Associate
  • 932 Views
  • 0 replies
  • 0 kudos

Flashing and debugging STM32F103C

Hello Everyone,I got a new board for then  STM32F103C and I want to debug as well as dump code.I connect the BOOT0 to GND, and connect the respective pins of STLink (Nrst Pin- NC).However I am not able to do anything.It gives hardFault error

Abhi1 by Associate II
  • 4754 Views
  • 8 replies
  • 0 kudos

I2C problem with STM32L476RGT6(NUCLEO-L476RG)

Hi,I am using NUCLEO-L476RG. I have wrote below code using HAL library to toggle an LED via I2C. But I cant find my board address.Kindly let me know how to find it.MX_I2C1_Init(); /* USER CODE BEGIN 2 */ if (HAL_I2C_IsDeviceReady(&hi2c1,????????,2,10...

spark by Associate II
  • 1590 Views
  • 2 replies
  • 0 kudos