STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unknown pulsing on STM32L073RZ

Hi there,I'm working with an STM32L073RZ CPU and Mbed OS 5.12.0 and experiencing an issue that I'm not quite sure how to describe. The processor gets into a state whereby it oscillates a pin (PA_5 which is setup as an InterruptIn that pulls down) and...

0690X000008j8PjQAI.png

Problem with STM32F4.7 External Interrupt

Dear All,i configured an input pin as external interrupt with rising edge detection and pulled it down internally.i apply a pulse train which it sets and resets within the time that the interrupt is disabled.i expect that the ISR executes when it is ...

RShar.17 by Associate II
  • 1712 Views
  • 2 replies
  • 0 kudos

STM32F103 - PB3 just doesn't work as GPIO

Posted on December 14, 2016 at 10:27Hello,did anyone ever manage to get PB3 working as an I/O port on an STM32F103?I am having a hard time with the F103VB where I need PB3 as input - no matter what I try, PB3 simply is returning a 0 value.AFIO->MAPR...

tilmann by Associate III
  • 18094 Views
  • 32 replies
  • 1 kudos

SPI not working with MCP6S21

Hi everyone,I would like to use a simple VGA (MCP6S21) but still not reach to do it.The datasheet is available here : http://ww1.microchip.com/downloads/en/devicedoc/21117b.pdfI'd like to put a +2 gain, the signals (SCK,MOSI) I transmit seems to be O...

MJouv by Associate
  • 969 Views
  • 0 replies
  • 0 kudos

About UART communication between PC and STM32F4

Hey, I am trying to connect my STM32F4-DISC board to PC via USART. It is a very common and basic example like sending a string to PC COM port which is covered by lots of tutorials on the web. But my question is,I first used this product and directly ...

YAkse by Associate III
  • 1092 Views
  • 1 replies
  • 0 kudos