STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Open-Drain output connected to WKUP pin

Hi,I'm working with an STM32L073RZ on a custom board, using MbedOS 5.12.0 bare metal. The board is a very low power weigh scale that is normally in Standby mode and is awoken by an accelerometer (connected to PC_13), an NFC chip (connected to PA_0). ...

Resolved! STM32F429ZI aborting DMA transfer on USART3 prematurely

On an STM32F429ZI, I'm using USART3_RX to receive information via DMA into a circular buffer. The buffer is 4096 bytes long.If I send 1 or 2 bytes at a time (i.e. with a delay of ~100ms+ between transfers), things work correctly. By "work correctly" ...

TDK by Super User
  • 2239 Views
  • 4 replies
  • 0 kudos

Timer synchronization still has offset

Hello,I am trying to synchronize two PWM outputs on an STM32H7: TIM4 channel 2 and TIM8 channel 3N.To do this I am using the HAL synchronization functions, setting TIM4 up as master with "HAL_TIMEx_MasterConfigSynchronization" and TIM8 with "HAL_TIM_...

ST User by Associate III
  • 2254 Views
  • 3 replies
  • 0 kudos

Where is the VREFINT_CAL for STM32L072z

Hi everyone ! I read in the datasheet that I need the VREFINT_CAL to calculate my real VDDA but I don't find it in the datasheet. In every other model's datasheet you can find the VREFINT_CAL easily but not in the STM32L0 one. Is someone kno...

YMAIL by Associate II
  • 1561 Views
  • 2 replies
  • 0 kudos

Resolved! A question about Vdd, VddA, Vref and clock frequencies

Hello,we want to build a system with STM32H7, hopefully one of the new up to 480 MHz devices. And we really need a high clock of 400 MHz and above. On the other hand we need low power and we use ADC and DAC, both requiring a 3.3V Vref.Now my question...

ADC accuracy problem

I am sensing the voltage using stm32f103c8 module.using Keil micro--vision 5register level codingcode:#include "stm32f10x.h"       float av,volt; int main(void) { // SEND A CLOCK SOURCE FOR ADC //LcdSend2StringWithDelay(50000,"Start Clock",""); ...

Bud by Associate III
  • 3102 Views
  • 8 replies
  • 0 kudos

Unknown pulsing on STM32L073RZ

Hi there,I'm working with an STM32L073RZ CPU and Mbed OS 5.12.0 and experiencing an issue that I'm not quite sure how to describe. The processor gets into a state whereby it oscillates a pin (PA_5 which is setup as an InterruptIn that pulls down) and...

0690X000008j8PjQAI.png